STM32 Canbus Multiple Device Weird İssue
I am developing a project with STM32 using the STM32G473CET6 chip and working on a CAN bus system. In this project, the STM32 sends messages to the bus, processes the received messages, and responds accordingly. For example, the message 10170001 queries the I/Os states of device 01, and the response consists of 8 messages containing the I/Os,dev states, PWM values, etc. However, if there are multiple devices on the bus, when I query device 02 with the message 10170002, it seems to print some of the responses from the previously sent message 10170001 (e.g., 2 out of the 8 messages). Then, on the third query, it finally sends the correct I/O states of device 02. It feels like there is some kind of overflow or buffering issue within the STM32, but when I check the FIFO levels, everything seems fine. My termination resistors are also properly configured. What could be causing this strange behavior? thank you
1 - My termination resistors are correctly placed at both ends of the bus. 2 - I have implemented mechanisms to monitor FIFO levels. 3 - I used an analyzer to track the messages on the bus. 4 - I don't think this is a hardware issue, as the same problem occurs on both devices. 5 - My CAN bus speed is 500 kbps, but I am observing this issue even when sending a low number of test messages on the bus.
/* main can line fifo0 callback */
void HAL_FDCAN_RxFifo0Callback(FDCAN_HandleTypeDef *hfdcan, uint32_t RxFifo0ITs)
{
FDCAN_RxHeaderTypeDef bufRxHdrCan;
uint8_t payloadCan[8];
if ((RxFifo0ITs & FDCAN_IT_RX_FIFO0_NEW_MESSAGE) != RESET)
{
if (HAL_FDCAN_GetRxMessage(hfdcan, FDCAN_RX_FIFO0,&bufRxHdrCan,payloadCan) == HAL_OK)
{
dbgPrintf("Can1 new message in RxFifo0\n");
dbgPrintf("RxHeader.Identifier: %x\n", bufRxHdrCan.Identifier);
dbgPrintf("RxHeader.DataLength: %x\n", bufRxHdrCan.DataLength);
CanMessage canMsg;
memcpy(canMsg.data,payloadCan,bufRxHdrCan.DataLength);
canMsg.id = bufRxHdrCan.Identifier;
canMsg.len = bufRxHdrCan.DataLength;
ParsedID id = canMessageParseId(canMsg.id);
dbgTrace("ParsedID.pgn : %d\n", id.pgn);
dbgTrace("ParsedID.sourceAddr: %d\n", id.sourceAddr);
dbgTrace("ParsedID.targetAddr: %d\n", id.targetAddr);
if((id.targetAddr == gAppSettings.devAddress) || (id.targetAddr == BROADCAST_ADDRESS))
{
gSysMsg sysMsg;
sysMsg.dataDesc.msgId = canMsg.id;
sysMsg.dataDesc.msgsrc=SRC_CANA;
sysMsg.dataLen = canMsg.len;
memcpy(sysMsg.dataBuffer,payloadCan,sysMsg.dataLen);
gRingBufPush(&sysMsgRingBuf,(void*)(&sysMsg));
}
return;
}
dbgPrintf("ERROR: Fifo0Callback HAL_FDCAN_GetRxMessage\n");
Error_Handler(1); // id 1
}
}
/* can message send */
bool canMessageSend(CanLine cLine,CanMessage *pCanMsg)
{
FDCAN_HandleTypeDef *phfdcan = phfdcanMain;
FDCAN_TxHeaderTypeDef TxHeader;
TxHeader.Identifier = pCanMsg->id;
TxHeader.DataLength = pCanMsg->len;
TxHeader.IdType = FDCAN_EXTENDED_ID;
if(TxHeader.DataLength > 0)
{
TxHeader.TxFrameType = FDCAN_DATA_FRAME;
}
else
{
TxHeader.TxFrameType = FDCAN_REMOTE_FRAME;
}
TxHeader.ErrorStateIndicator = FDCAN_ESI_PASSIVE;
TxHeader.BitRateSwitch = FDCAN_BRS_OFF;
TxHeader.FDFormat = FDCAN_CLASSIC_CAN;
TxHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS;
TxHeader.MessageMarker = 0;
dbgTrace("canMessageSend\n");
dbgTrace("id = %d\n", pCanMsg->id);
dbgTrace("len = %d\n",pCanMsg->len);
while (HAL_FDCAN_GetTxFifoFreeLevel(phfdcan) == 0);
if (HAL_FDCAN_AddMessageToTxFifoQ(phfdcan,&TxHeader,pCanMsg->data)!= HAL_OK)
{
dbgPrintf("ERROR:HAL_FDCAN_AddMessageToTxFifoQ-MIO\n");
return false;
}
return true;
}