STM32 Cube IDE: Reset_Handler() at 0x80021e0
Hi STM team,
I am using the STM32WL55CCU6 MCU on a custom PCB project. I actually have two of these. One is working as a master, while the other operates as a slave. My slave device is working properly, but the master is not.
Problem Statement: When debugging, a tab appears with the information: "Reset_Handler() at 0x80021e0". Attached is a screenshot. I am not sure what is causing this, but I think it is blocking my code from executing properly because when I place breakpoints at the printf() and APP_LOG() debugging statements, these do not execute, and no output is shown on the terminal.
Note: under Properties > C/C++ Build > Settings MCU GCC Assembler > Debugging I have set to maximum (-g3). Under MCU GCC Compiler > Optimization I have set to None (-O0).
When I change these configurations to default (-g) and optimize for Debug (-Og) respectively, the warning tab that appears changes to: "main() at 0x8000a94". Attached is a 2nd screenshot depicting this.
I am using STMCubeIDE Version 1.14.0 I have included a 3rd photo showing the software versions I am using. I have double checked my pin configurations, clock settings and there are no errors or warnings that show up after building. I have looked at the online forums and I can't find anything helpful. Is there anyone that can help me troubleshoot this issue? It is time sensitive, and I am a software developer for a company. We are customers of ST. If there is another way to get in contact with an ST FAE, I would appreciate that information as well.
Please let me know if there is any other relevant information I can provide.
Thank you for any support in advance,
-Jake