Skip to main content
Visitor II
October 22, 2020
Question

STM32 + EXPHY USB3300 + VBUS Sensing

  • October 22, 2020
  • 0 replies
  • 576 views

Dear All.

Based on HAL library, I make small project where I have USB HS with external PHY (USB3300) and CDC class. Works well. What I need is to implement Vbus sensing. This can be done only via external phy, there are some flags in registers to enable it, but I don’t know how make it working. I got a few question:

1.      Can current HAL library enable vbus sensing in the USB3300 chip?

2.      Is it possible to have access to the ULPI communication to setup those registers and bit manually?

BR

KWT

    This topic has been closed for replies.