STM32 SDK 1.24.0 fails to reconnect HID-Usb on PC reboot
I have got the following problem:
I am working with VisualGDB and updated my STM32 SDK from 1.23.0 to 1.24.0 and now, our device looses USB connection when the host PC restarts and doesn’t reconnect.
Th device sends a report every 5ms to the PC via USBD_CUSTOM_HID_SendReport. This seems to be the problem, as when i delete the line the device is reconnected.
I was able to reproduce this in an tutorial project using the following:
main.cpp
#ifdef __cplusplus
extern "C"
{
#endif
#include <usbd_core.h>
#include <usbd_customhid.h>
#include "usbd_customhid_if.h"
#include <usbd_desc.h>
USBD_HandleTypeDef USBD_Device;
void SysTick_Handler(void);
void OTG_FS_IRQHandler(void);
void OTG_HS_IRQHandler(void);
extern PCD_HandleTypeDef hpcd;
#ifdef __cplusplus
}
#endif
static void SystemClock_Config(void)
{
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_OscInitTypeDef RCC_OscInitStruct;
__PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 8;
RCC_OscInitStruct.PLL.PLLN = 336;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 7;
HAL_RCC_OscConfig(&RCC_OscInitStruct);
RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK |
RCC_CLOCKTYPE_HCLK |
RCC_CLOCKTYPE_PCLK1 |
RCC_CLOCKTYPE_PCLK2);
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5);
}
void SysTick_Handler(void)
{
HAL_IncTick();
HAL_SYSTICK_IRQHandler();
}
#ifdef USE_USB_FS
void OTG_FS_IRQHandler(void)
{
HAL_PCD_IRQHandler(&hpcd);
}
#elif defined(USE_USB_HS)
void OTG_HS_IRQHandler(void)
{
HAL_PCD_IRQHandler(&hpcd);
}
#else
#error USB peripheral type not defined
#endif
/*
This is a basic USB CDC device sample based on the ST USB library.
To test it out:
1. Install the ST VCP drivers (http://www.st.com/web/en/catalog/tools/PF257938)
2. Connect to the virtual COM port using SmarTTY or any other terminal program
3. Type some characters and observe the output
Read more about the sample: http://visualgdb.com/tutorials/arm/stm32/usb/
*/
int main(void)
{
HAL_Init();
SystemClock_Config();
USBD_Init(&USBD_Device, &VCP_Desc, 0);
USBD_RegisterClass(&USBD_Device, USBD_CUSTOM_HID_CLASS);
USBD_CUSTOM_HID_RegisterInterface(&USBD_Device, &USBD_CUSTOM_HID_Test_fops);
USBD_Start(&USBD_Device);
HAL_Delay(1000);
for (;;)
{
if (USBD_Device.dev_state == USBD_STATE_CONFIGURED)
{
uint8_t test[] = { 1,0,0,0 };
USBD_CUSTOM_HID_SendReport(&USBD_Device, test, sizeof(test));
}
HAL_Delay(10);
}
}usb_customhid_if.h
#pragma once
#ifdef __cplusplus
extern "C" {
#endif
#include "usbd_customhid.h"
extern __ALIGN_BEGIN uint8_t m_hidReportDescription[] __ALIGN_END;
extern USBD_CUSTOM_HID_ItfTypeDef USBD_CUSTOM_HID_Test_fops;
#ifdef __cplusplus
}
#endifusb_customhid_if.c
#include "usbd_customhid_if.h"
static int8_t BSP_Test_Init(void);
static int8_t BSP_Test_DeInit(void);
static int8_t BSP_Test_Control(uint8_t event_idx, uint8_t state);
uint8_t m_hidReportDescription[USBD_CUSTOM_HID_REPORT_DESC_SIZE] = {
/* 7 bytes */
0x06, 0x00, 0xff, // USAGE_PAGE (Vendor Defined Page 1)
0x09, 0x01, // USAGE (Vendor Usage 1)
0xa1, 0x01, // COLLECTION (Application)
/* 19 bytes */
0x85, 1, // REPORT_ID (1)
0x09, 0x3b, // USAGE (Byte Count)
0x15, 0x00, // LOGICAL_MINIMUM (0)
0x26, 0xff, 0x00, // LOGICAL_MAXIMUM (255)
0x95, 3, // REPORT_COUNT (17)
0x75, 0x08, // REPORT_SIZE (8)
0x81, 0x02, // INPUT (Data,Var,Abs)
0x09, 0x3b, // USAGE (Byte Count)
0x91, 0x02, // OUTPUT (Data,Var,Abs)
/* 1 bytes */
0xc0 // END_COLLECTION
};
USBD_CUSTOM_HID_ItfTypeDef USBD_CUSTOM_HID_Test_fops =
{
m_hidReportDescription,
BSP_Test_Init,
BSP_Test_DeInit,
BSP_Test_Control
};
extern USBD_HandleTypeDef USBD_Device;
static int8_t BSP_Test_Init(void)
{
printf("hid_fops_init()\n");
return (0);
}
static int8_t BSP_Test_DeInit(void)
{
printf("hid_fops_deinit()\n");
return (0);
}
static int8_t BSP_Test_Control(uint8_t event_idx, uint8_t state)
{
return (0);
}This outputs:
hid_fops_init()
<Rebooting Host PC here >
hid_fops_deinit()
hid_fops_init()
hid_fops_deinit()Setup:
Board: STM32F407VG
VisualGDB: 5.5 Preview 1
BSP: 2019.06 (= SDK 1.24.0)
ARM ToolChain: 9.21/8.3.0/r1
Packages:
– STM32F4 HAL Library
– STM32F4 Low-level Driver Library
– STM32 USB Device Library – Custom Human Interface Device
– Fast Semihosting and Embedded Profiler