Skip to main content
Visitor II
October 21, 2020
Question

STM32 USB Host Class CDC missing size check for buffer

  • October 21, 2020
  • 0 replies
  • 667 views

The function USBH_CDC_Receive should check that the parameter length is a multiple of endpoint size.

Reason for this that CDC_ProcessReception calls USBH_BulkReceiveData with the argument CDC_Handle->DataItf.InEpSize. So if the argument pbuff passed to USBH_CDC_Receive points to a buffer smaller than the endpoint size USBH_BulkReceiveData will write over the buffer end.

See also for a additional problem with CDC_ProcessReception.

EDIT:

Found another problem. "phost->pActiveClass->Name" is a argument but there is no "%s" in the format string.

USBH_DbgLog("Cannot Find the interface for Communication Interface Class.", phost->pActiveClass->Name);

Hope this is not a mistake of my side.

    This topic has been closed for replies.