STM32 USB Host. Virtual Port Com. FTDI and CH340
I use the stm32g0b1 microcontroller to USB Host. I use the HAL library from STMicroelectronics. Class for FS IP: Communication Host Class (Virtual Port Com). And it works great with other microcontrollers that use Class for FS IP: Communication Device Class (Virtual Port Com). Both from ST and from other companies. But if I connect a device from FTDI (for example FT230X or FT232) or from WCH (for example CH340/343) to the host, nothing works. Everything freezes on Appli_state == APPLICATION_START.
As far as I understand, many people have encountered this, but I have not found any solution to this on the Internet. Is it possible to somehow change the standard library for USB Host from ST so that it would be possible to connect such devices?