STM32 USBD MIC AND STREAMING AUDIO
I am configuring USBD to turn the STM32F4 Discovery into a headphone, meaning it can play music through USB and transmit data from the PDM microphone to the computer. I have completed the music playback part, but I am now working on the recording part and don't know how to configure USBD audio. Can you help me?
#ifndef USE_USBD_COMPOSITE
/* USB AUDIO device Configuration Descriptor */
__ALIGN_BEGIN static uint8_t USBD_AUDIO_CfgDesc[USB_AUDIO_CONFIG_DESC_SIZ] __ALIGN_END =
{
/* Configuration 1 */
0x09, /* bLength */
USB_DESC_TYPE_CONFIGURATION, /* bDescriptorType */
LOBYTE(USB_AUDIO_CONFIG_DESC_SIZ), /* wTotalLength */
HIBYTE(USB_AUDIO_CONFIG_DESC_SIZ),
0x02, /* bNumInterfaces */
0x01, /* bConfigurationValue */
0x00, /* iConfiguration */
#if (USBD_SELF_POWERED == 1U)
0xC0, /* bmAttributes: Bus Powered according to user configuration */
#else
0x80, /* bmAttributes: Bus Powered according to user configuration */
#endif /* USBD_SELF_POWERED */
USBD_MAX_POWER, /* MaxPower (mA) */
/* 09 byte*/
/* USB Speaker Standard interface descriptor */
AUDIO_INTERFACE_DESC_SIZE, /* bLength */
USB_DESC_TYPE_INTERFACE, /* bDescriptorType */
0x00, /* bInterfaceNumber */
0x00, /* bAlternateSetting */
0x00, /* bNumEndpoints */
USB_DEVICE_CLASS_AUDIO, /* bInterfaceClass */
AUDIO_SUBCLASS_AUDIOCONTROL, /* bInterfaceSubClass */
AUDIO_PROTOCOL_UNDEFINED, /* bInterfaceProtocol */
0x00, /* iInterface */
/* 09 byte*/
/* USB Speaker Class-specific AC Interface Descriptor */
AUDIO_INTERFACE_DESC_SIZE, /* bLength */
AUDIO_INTERFACE_DESCRIPTOR_TYPE, /* bDescriptorType */
AUDIO_CONTROL_HEADER, /* bDescriptorSubtype */
0x00, /* 1.00 */ /* bcdADC */
0x01,
0x27, /* wTotalLength */
0x00,
0x01, /* bInCollection */
0x01, /* baInterfaceNr */
/* 09 byte*/
/* USB Speaker Input Terminal Descriptor */
AUDIO_INPUT_TERMINAL_DESC_SIZE, /* bLength */
AUDIO_INTERFACE_DESCRIPTOR_TYPE, /* bDescriptorType */
AUDIO_CONTROL_INPUT_TERMINAL, /* bDescriptorSubtype */
0x01, /* bTerminalID */
0x01, /* wTerminalType speaker 0x0201 */
0x02,
0x00, /* bAssocTerminal */
0x01, /* bNrChannels */
0x00, /* wChannelConfig 0x0000 Mono */
0x00,
0x00, /* iChannelNames */
0x00, /* iTerminal */
/* 12 byte*/
/* USB Speaker Audio Feature Unit Descriptor */
0x09, /* bLength */
AUDIO_INTERFACE_DESCRIPTOR_TYPE, /* bDescriptorType */
AUDIO_CONTROL_FEATURE_UNIT, /* bDescriptorSubtype */
AUDIO_OUT_STREAMING_CTRL, /* bUnitID */
0x01, /* bSourceID */
0x01, /* bControlSize */
AUDIO_CONTROL_MUTE, /* bmaControls(0) */
0, /* bmaControls(1) */
0x00, /* iTerminal */
/* 09 byte */
/* USB Speaker Output Terminal Descriptor */
0x09, /* bLength */
AUDIO_INTERFACE_DESCRIPTOR_TYPE, /* bDescriptorType */
AUDIO_CONTROL_OUTPUT_TERMINAL, /* bDescriptorSubtype */
0x03, /* bTerminalID */
0x01, /* wTerminalType 0x0101 stream audio*/
0x031,
0x00, /* bAssocTerminal */
0x02, /* bSourceID */
0x00, /* iTerminal */
/* 09 byte */
/* USB Speaker Standard AS Interface Descriptor - Audio Streaming Zero Bandwidth */
/* Interface 1, Alternate Setting 0 */
AUDIO_INTERFACE_DESC_SIZE, /* bLength */
USB_DESC_TYPE_INTERFACE, /* bDescriptorType */
0x01, /* bInterfaceNumber */
0x00, /* bAlternateSetting */
0x00, /* bNumEndpoints */
USB_DEVICE_CLASS_AUDIO, /* bInterfaceClass */
AUDIO_SUBCLASS_AUDIOSTREAMING, /* bInterfaceSubClass */
AUDIO_PROTOCOL_UNDEFINED, /* bInterfaceProtocol */
0x00, /* iInterface */
/* 09 byte*/
/* USB Speaker Standard AS Interface Descriptor - Audio Streaming Operational */
/* Interface 1, Alternate Setting 1 */
AUDIO_INTERFACE_DESC_SIZE, /* bLength */
USB_DESC_TYPE_INTERFACE, /* bDescriptorType */
0x01, /* bInterfaceNumber */
0x01, /* bAlternateSetting */
0x01, /* bNumEndpoints */
USB_DEVICE_CLASS_AUDIO, /* bInterfaceClass */
AUDIO_SUBCLASS_AUDIOSTREAMING, /* bInterfaceSubClass */
AUDIO_PROTOCOL_UNDEFINED, /* bInterfaceProtocol */
0x00, /* iInterface */
/* 09 byte*/
/* USB Speaker Audio Streaming Interface Descriptor */
AUDIO_STREAMING_INTERFACE_DESC_SIZE, /* bLength */
AUDIO_INTERFACE_DESCRIPTOR_TYPE, /* bDescriptorType */
AUDIO_STREAMING_GENERAL, /* bDescriptorSubtype */
0x01, /* bTerminalLink */
0x01, /* bDelay */
0x01, /* wFormatTag AUDIO_FORMAT_PCM 0x0001 */
0x00,
/* 07 byte*/
/* USB Speaker Audio Type III Format Interface Descriptor */
0x0B, /* bLength */
AUDIO_INTERFACE_DESCRIPTOR_TYPE, /* bDescriptorType */
AUDIO_STREAMING_FORMAT_TYPE, /* bDescriptorSubtype */
AUDIO_FORMAT_TYPE_I, /* bFormatType */
0x02, /* bNrChannels */
0x02, /* bSubFrameSize : 2 Bytes per frame (16bits) */
16, /* bBitResolution (16-bits per sample) */
0x01, /* bSamFreqType only one frequency supported */
AUDIO_SAMPLE_FREQ(USBD_AUDIO_FREQ), /* Audio sampling frequency coded on 3 bytes */
/* 11 byte*/
/* Endpoint 1 - Standard Descriptor */
AUDIO_STANDARD_ENDPOINT_DESC_SIZE, /* bLength */
USB_DESC_TYPE_ENDPOINT, /* bDescriptorType */
AUDIO_OUT_EP, /* bEndpointAddress 1 out endpoint */
USBD_EP_TYPE_ISOC, /* bmAttributes */
AUDIO_PACKET_SZE(USBD_AUDIO_FREQ), /* wMaxPacketSize in Bytes (Freq(Samples)*2(Stereo)*2(HalfWord)) */
AUDIO_FS_BINTERVAL, /* bInterval */
0x00, /* bRefresh */
0x00, /* bSynchAddress */
/* 09 byte*/
/* Endpoint - Audio Streaming Descriptor */
AUDIO_STREAMING_ENDPOINT_DESC_SIZE, /* bLength */
AUDIO_ENDPOINT_DESCRIPTOR_TYPE, /* bDescriptorType */
AUDIO_ENDPOINT_GENERAL, /* bDescriptor */
0x00, /* bmAttributes */
0x00, /* bLockDelayUnits */
0x00, /* wLockDelay */
0x00,
/* 07 byte*/
} ;
/* USB Standard Device Descriptor */
__ALIGN_BEGIN static uint8_t USBD_AUDIO_DeviceQualifierDesc[USB_LEN_DEV_QUALIFIER_DESC] __ALIGN_END =
{
USB_LEN_DEV_QUALIFIER_DESC,
USB_DESC_TYPE_DEVICE_QUALIFIER,
0x00,
0x02,
0x00,
0x00,
0x00,
0x40,
0x01,
0x00,
}; it's i my config