STM32C031 Reseting after receiving data on UART
Hello, I'm having problems with a simple task: receive blocks of data from UART. The blocks are sequences of 1-300 bytes, that are receiveid with a 1 second interval. The value is stored in one buffer of 350 bytes.
When I send a big block of 270 bytes after other blocks(of 60 bytes by example) in that 1s interval, the Stm32 RESETS! But if the interval is longer, like 5 seconds, it doesn't reset and receive the data correctly.
I tried with pooling and interruption, the result is the same. I'm using 115200 baud. Lowering the baud rate also reduces the interval that doesn't cause a reset, but I can't use this solution.
WatchDog is already disabled. By this moment, the code doesn't do anything more.