STM32C071 bootloader patterns and boot selector bits defaults
Hello,
I am currently working on a small device with a C071GBU. This is the first time I am using a chip with shared pins (PA12/PA10 and PA11/PA9) as well as no dedicated single-function BOOT0 pin.
My PCB has very tight space constraints, so software debugger or programming pads are no option - everything must work via the USB port, from first time setup on.
If I understood the specsheet correctly ("Pins PA9 and PA10 can be remapped in place of pins PA11 and PA12 (default mapping), using SYSCFG_CFGR1 register"), PA12/PA11 are default (and not PA10/PA9), so a fresh chip out of the box can be used for USB DFU, am I correct in this assumption?
Then there is my next question - how does BOOT0 work? If I understand correctly, the boot selector bits decide whether PA14 is BOOT0, or whether a software bit is used. The patterns in AN2606 are as follows:

What I do not understand - how are the defaults? As in, if I have a fresh chip directly from the factory, how is it set up? Will PA14 operate as BOOT0 out of the box, or is this something I have to manually set in a first-time-flash? If the flash memory is empty the chip should always default to entering the bootloader, so I can flash a firmware that sets the correct bits through USB, and from there on PA14 is BOOT0, correct? I am sorry for asking questions that may seem trivial - bootloader patterns have been confusing me before, and I would prefer a prototype that works at least well enough to test all important features. This is a personal project, so prototyping funds are limited.
Then I have one third and hopefully last question - If PA14 is set up as BOOT0, can it still be used as a regular GPIO once the chip booted from the program flash memory? Background: The PCB has a single button. If the user holds this button while plugging in the device, it should enter bootloader. Once the chip has booted successfully, this button is however supposed to be used as part of the user interface to interact with the PCB. If the button can work as BOOT0 during startup, and then PA14 as soon as the boot from internal flash is completed, it would simplify my design. My workaround would be to short PA14 to PA13, and use PA13 after startup.
Kind regards,
Moritz