Skip to main content
Graduate
October 4, 2025
Solved

STM32Cube MCU Package for STM32U0 Series 1.3.0 (Doxygen error)

  • October 4, 2025
  • 1 reply
  • 238 views

File: stm32u0xx_hal_gpio.c

/**
 * @brief Lock GPIO Pins configuration registers.
 * @note The locked registers are GPIOx_MODER, GPIOx_OTYPER, GPIOx_OSPEEDR,
 * GPIOx_PUPDR, GPIOx_AFRL and GPIOx_AFRH.
 * @note The configuration of the locked GPIO pins can no longer be modified
 * until the next reset.
 * @PAram GPIOx where x can be (A..F) to select the GPIO peripheral for STM32U0xx family
 * @PAram GPIO_Pin specifies the port bits to be locked.
 * This parameter can be any combination of GPIO_Pin_x where x can be (0..15).
 * @retval None
 */
HAL_StatusTypeDef HAL_GPIO_LockPin(GPIO_TypeDef *GPIOx, uint16_t GPIO_Pin)
{

HAL_GPIO_LockPin() should return HAL_StatusTypeDef.

But in Doxygen None

ATret3_0-1759612532143.png

 

    This topic has been closed for replies.
    Best answer by Saket_Om

    Hello @ATret.3 

    Thank you for bringing this issue to our attention.

    I reported this internally.

    Internal ticket number: 218966 (This is an internal tracking number and is not accessible or usable by customers).

    1 reply

    Saket_OmAnswer
    Technical Moderator
    October 6, 2025

    Hello @ATret.3 

    Thank you for bringing this issue to our attention.

    I reported this internally.

    Internal ticket number: 218966 (This is an internal tracking number and is not accessible or usable by customers).