STM32CubeMX - V6.12.0 CAN-FD Transciever Delay Compensation & Auto Retransmission
Hi,
I'm currently using STM32CubeMX V6.12.0 to initialise the peripherals on an STM32H753 processor, and I had a couple of questions:
1. How do I enable & then configure the CAN Transciever Delay Compensation within CubeMX?
2. Is there a mechanism for limiting the number of auto-retransmissions in the event of a CAN Error? I currently have that option unchecked but when doing bench-top testing it's clogging up the processor and causing it to run slowly.
Many Thanks,
Crispin