STM32F-407G-Disc1 booting only right after firmware flashing.
Hi
I am working on an audio application (see http://ixox.fr/forum/index.php?topic=63425.45) and I am experiencing an issue:
- when I just flash the app, whilst still plugged in on my desktop, the app boots and works fine.
- When I power the board without a PC connection, it keeps blinking slowly red on LD1and nothing happens.
My board is a STM32F407G-Disc1 , serial being : MB995-D-01 / 218509479.
I have found many people describing similar issues: explanation the ST-LINK firmware pulls the NRST Low etc...
None of their proposed workarounds seems to work ...
I already
- tried removing SB11 blob -- no good -- set it back.
- pulling RST to 3.3V through a resistor -- not convincing.
- upgraded the ST-Link firmware to the most recent version V2J36M26, tries several available versions (2.32; 2.33). Some people mention the 2.24 or 2.25 being OK but they seem not available.
I am lost.
I would need it to work soon as is is intended as a gift for my son who studies electronic music before he returns to his college :(
Has anyone a method that works?
In absence of any working way, the interest of that board is dramatically reduced.
Regards
Dominique