STM32F series - USB Peripheral Requirements - Communicate With Windows Application
Hello, I am wanting to build a project that consists a STM32 "F" or "L" series MCU, and I want to use the USB Peripheral from within STM32CubeMX. I want to create a windows application using Microsoft Visual Studios (C#), and have communication back and forth between the STM32 MCU and the windows application.
These are my specific questions regarding this:
- It looks like any F or L series is capable of this, and has the USB Peripheral available via STM32CubeMX is that right?
- Are there any hardware requirements to make the USB Peripheral work? I'm guessing I need to use a precise external clock, but I cannot find specific information on this application. Or will the internal clock work for this?
- The USB Peripheral will allow the STM32 to show up as a virtual USB com port, e.g. under device manager it should show up under "Ports" as "USB Serial Device (COMX)". Do you know how to have a custom name for this?
Thanks and any help or advice is greatly appreciated!