STM32F030 outputs 1.3V instead of 3V
I have set all GPIOB ports as outputs and have an adjustable resistor on port PA1 which I’ve set as an analogue input to do an adc conversion to display a voltage output to three seven segment displays with each segment being connected from PB0 to PB6 however it seems my port B pins are not outputting a voltage of 3V when set to high. All ports are set as pull downs internally. What could be the reason for this?