Solved
STM32F030K6 _ external interrupt just 1/3 EXT line is function
Hi,
I try to use 6 external interrupts but only EXT4_15 is functionning. All is functionning correctly when i use HAL_GPIO_ReadPin() function without interrupts.
Thank you for your HELP

void EXTI0_1_IRQHandler(void)
{
/* USER CODE BEGIN EXTI0_1_IRQn 0 */
/* USER CODE END EXTI0_1_IRQn 0 */
HAL_GPIO_EXTI_IRQHandler(EV5_Pin);
HAL_GPIO_EXTI_IRQHandler(EV6_Pin);
/* USER CODE BEGIN EXTI0_1_IRQn 1 */
/* USER CODE END EXTI0_1_IRQn 1 */
}
/**
* @brief This function handles EXTI line 2 and 3 interrupts.
*/
void EXTI2_3_IRQHandler(void)
{
/* USER CODE BEGIN EXTI2_3_IRQn 0 */
/* USER CODE END EXTI2_3_IRQn 0 */
HAL_GPIO_EXTI_IRQHandler(EV89_Pin);
/* USER CODE BEGIN EXTI2_3_IRQn 1 */
/* USER CODE END EXTI2_3_IRQn 1 */
}
/**
* @brief This function handles EXTI line 4 to 15 interrupts.
*/
void EXTI4_15_IRQHandler(void)
{
/* USER CODE BEGIN EXTI4_15_IRQn 0 */
/* USER CODE END EXTI4_15_IRQn 0 */
HAL_GPIO_EXTI_IRQHandler(EV2_Pin);
HAL_GPIO_EXTI_IRQHandler(EV14_Pin);
HAL_GPIO_EXTI_IRQHandler(EV3_Pin);
/* USER CODE BEGIN EXTI4_15_IRQn 1 */
/* USER CODE END EXTI4_15_IRQn 1 */
}The main.c with the callback function
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2025 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/*Paramètres systèmes*/
#define spike_voltage 24 /*Volts*/
#define spike_duration 20 /*ms*/
#define hold_voltage 9 /*Volts*/
/*Paramètres internes logiciels*/
/*Paramètres PWM pour Fclk = 16Mhz PSC = 0 soit FPWM 6024 Hz*/
#define ARR 2655
#define CRR_spike 2655
#define CRR_hold ((hold_voltage* ARR / spike_voltage))
/*#define CRR_hold 996*/
volatile uint8_t cons_EV14_active = 0;
volatile uint8_t cons_EV2_active = 0;
volatile uint8_t cons_EV3_active = 0;
volatile uint8_t cons_EV89_active = 0;
volatile uint8_t cons_EV5_active = 0;
volatile uint8_t cons_EV6_active = 0;
volatile uint32_t t14 = 0;
volatile uint32_t t2 = 0;
volatile uint32_t t3 = 0;
volatile uint32_t t89 = 0;
volatile uint32_t t5 = 0;
volatile uint32_t t6 = 0;
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
TIM_HandleTypeDef htim1;
TIM_HandleTypeDef htim3;
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_TIM1_Init(void);
static void MX_TIM3_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_TIM1_Init();
MX_TIM3_Init();
/* USER CODE BEGIN 2 */
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_2);
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1);
HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_2);
HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_1);
HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_4);
HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_3);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/*EV14*/
if (cons_EV14_active == 1) {
if (HAL_GetTick() - t14 < spike_duration) {
TIM1->CCR2 = CRR_spike;
} else {
TIM1->CCR2 = CRR_hold;
}
} else {
TIM1->CCR2 = 0;
}
/*EV2*/
if (cons_EV2_active == 1) {
if (HAL_GetTick() - t2 < spike_duration) {
TIM1->CCR1 = CRR_spike;
} else {
TIM1->CCR1 = CRR_hold;
}
} else {
TIM1->CCR1 = 0;
}
/*EV3*/
if (cons_EV3_active == 1) {
if (HAL_GetTick() - t3 < spike_duration) {
TIM3->CCR2 = CRR_spike;
} else {
TIM3->CCR2 = CRR_hold;
}
} else {
TIM3->CCR2 = 0;
}
/*EV89*/
if (cons_EV89_active == 1) {
if (HAL_GetTick() - t89 < spike_duration) {
TIM3->CCR1 = CRR_spike;
} else {
TIM3->CCR1 = CRR_hold;
}
} else {
TIM3->CCR1 = 0;
}
/*EV5*/
if (cons_EV5_active == 1) {
if (HAL_GetTick() - t5 < spike_duration) {
TIM3->CCR4 = CRR_spike;
} else {
TIM3->CCR4 = CRR_hold;
}
} else {
TIM3->CCR4 = 0;
}
/*EV6*/
if (cons_EV6_active == 1) {
if (HAL_GetTick() - t6 < spike_duration) {
TIM3->CCR3 = CRR_spike;
} else {
TIM3->CCR3 = CRR_hold;
}
} else {
TIM3->CCR3 = 0;
}
HAL_Delay(1);
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) {
switch(GPIO_Pin)
{
/*EV14*/
case EV14_Pin :
if (!HAL_GPIO_ReadPin(GPIOA, EV14_Pin)) {
cons_EV14_active = 1;
TIM1->CCR2 = CRR_spike;
t14 = HAL_GetTick();
} else {
cons_EV14_active = 0;
TIM1->CCR2 = 0;
}
break;
/*EV2*/
case EV2_Pin :
if (!HAL_GPIO_ReadPin(GPIOA, EV2_Pin)) {
cons_EV2_active = 1;
TIM1->CCR1 = CRR_spike;
t2 = HAL_GetTick();
} else {
cons_EV2_active = 0;
TIM1->CCR1 = 0;
}
break;
/*EV3*/
case EV3_Pin :
if (!HAL_GPIO_ReadPin(GPIOA, EV3_Pin)) {
cons_EV3_active = 1;
TIM3->CCR2 = CRR_spike;
t3 = HAL_GetTick();
} else {
cons_EV3_active = 0;
TIM3->CCR2 = 0;
}
break;
/*EV89*/
case EV89_Pin :
if (!HAL_GPIO_ReadPin(GPIOA, EV89_Pin)) {
cons_EV89_active = 1;
TIM3->CCR1 = CRR_spike;
t89 = HAL_GetTick();
} else {
cons_EV89_active = 0;
TIM3->CCR1 = 0;
}
break;
/*EV5*/
case EV5_Pin :
if (!HAL_GPIO_ReadPin(GPIOA, EV5_Pin)) {
cons_EV5_active = 1;
TIM3->CCR4 = CRR_spike;
t5 = HAL_GetTick();
} else {
cons_EV5_active = 0;
TIM3->CCR4 = 0;
}
break;
/*EV6*/
case EV6_Pin :
if (!HAL_GPIO_ReadPin(GPIOA, EV6_Pin)) {
cons_EV6_active = 1;
TIM3->CCR3 = CRR_spike;
t6 = HAL_GetTick();
} else {
cons_EV6_active = 0;
TIM3->CCR3 = 0;
}
break;
}
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSE;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief TIM1 Initialization Function
* @PAram None
* @retval None
*/
static void MX_TIM1_Init(void)
{
/* USER CODE BEGIN TIM1_Init 0 */
/* USER CODE END TIM1_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};
/* USER CODE BEGIN TIM1_Init 1 */
/* USER CODE END TIM1_Init 1 */
htim1.Instance = TIM1;
htim1.Init.Prescaler = 0;
htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
htim1.Init.Period = 2655;
htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim1.Init.RepetitionCounter = 0;
htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_Init(&htim1) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 0;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_2) != HAL_OK)
{
Error_Handler();
}
sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
sBreakDeadTimeConfig.DeadTime = 0;
sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
if (HAL_TIMEx_ConfigBreakDeadTime(&htim1, &sBreakDeadTimeConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM1_Init 2 */
/* USER CODE END TIM1_Init 2 */
HAL_TIM_MspPostInit(&htim1);
}
/**
* @brief TIM3 Initialization Function
* @PAram None
* @retval None
*/
static void MX_TIM3_Init(void)
{
/* USER CODE BEGIN TIM3_Init 0 */
/* USER CODE END TIM3_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
/* USER CODE BEGIN TIM3_Init 1 */
/* USER CODE END TIM3_Init 1 */
htim3.Instance = TIM3;
htim3.Init.Prescaler = 0;
htim3.Init.CounterMode = TIM_COUNTERMODE_UP;
htim3.Init.Period = 2655;
htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
if (HAL_TIM_Base_Init(&htim3) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim3, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_Init(&htim3) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 0;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
if (HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_2) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_3) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_4) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM3_Init 2 */
/* USER CODE END TIM3_Init 2 */
HAL_TIM_MspPostInit(&htim3);
}
/**
* @brief GPIO Initialization Function
* @PAram None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOF_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pins : PA1 PA2 PA4 PA5
PA11 */
GPIO_InitStruct.Pin = GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_4|GPIO_PIN_5
|GPIO_PIN_11;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING_FALLING;
GPIO_InitStruct.Pull = GPIO_PULLUP;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* EXTI interrupt init*/
HAL_NVIC_SetPriority(EXTI4_15_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI4_15_IRQn);
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @PAram file: pointer to the source file name
* @PAram line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */