Skip to main content
Explorer II
November 25, 2022
Solved

STM32F091 internal bootloader support CAN?

  • November 25, 2022
  • 3 replies
  • 1135 views

Hi,

I studied the RM0091 (page 55). There UART, I2C is listed as supported interfaces for the internal bootloader.

I was wondering why the CAN isn't supported. Is this the case?

Thanks

    This topic has been closed for replies.
    Best answer by Peter BENSCH

    Correct, AN2606 lists all possible interfaces for the various STM32s, but there is no family with bootloader via CAN for the STM32F0 yet.

    Does it answer your question?

    Regards

    /Peter

    3 replies

    Technical Moderator
    November 25, 2022

    Correct, AN2606 lists all possible interfaces for the various STM32s, but there is no family with bootloader via CAN for the STM32F0 yet.

    Does it answer your question?

    Regards

    /Peter

    Mat1Author
    Explorer II
    November 25, 2022

    Yes, it does.

    Thank you for the prompt answer.

    Technical Moderator
    November 25, 2022

    You're welcome!

    If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

    Good luck!

    /Peter

    Graduate II
    November 25, 2022

    Before you happily jump into using the STM canbus bootloader, have it mind it WONT WORK if more than one canbus node is active.

    I realiced it the hard way https://community.st.com/s/question/0D53W00000apgoISAQ/is-the-stm-system-bootloader-trough-canbus-just-not-woking-when-more-than-one-device-shares-the-bus