STM32F103 CAN Arbitration lost
I have a problem using CAN on STM32F103C8T6. I use this MCU on a bluepill board,
a SN64HVD230 based CAN PHY and on the other end of the CAN bus a PiCAN2 board on
Raspberry Pi. I drew a picture to show my setup:
I want to have a 500 kbit/s-CAN-connection, I use the MCU with 16 MHz.
My initialization code (I use the STM32-HAL-API) for the CAN is the following:
#define CAN_RX_PORT GPIOA
#define CAN_RX_PIN LL_GPIO_PIN_11
#define CAN_TX_PORT GPIOA
#define CAN_TX_PIN LL_GPIO_PIN_12
void init_can_gpios(void){
LL_GPIO_SetPinMode(CAN_RX_PORT, CAN_RX_PIN, LL_GPIO_MODE_INPUT);
LL_GPIO_SetPinPull(CAN_RX_PORT,CAN_RX_PIN,LL_GPIO_PULL_UP);
LL_GPIO_SetPinMode(CAN_TX_PORT, CAN_TX_PIN, LL_GPIO_MODE_ALTERNATE);
LL_GPIO_SetPinSpeed(CAN_TX_PORT, CAN_TX_PIN, LL_GPIO_SPEED_FREQ_HIGH);
LL_GPIO_SetPinOutputType(CAN_TX_PORT,CAN_TX_PIN,LL_GPIO_OUTPUT_OPENDRAIN);
}
void init_can_periph(void){
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_CAN1);
__HAL_RCC_CAN1_CLK_ENABLE();
hcan1.Instance = CAN1;
hcan1.Init.Prescaler=2;
hcan1.Init.TimeSeg1=CAN_BS1_8TQ
hcan1.Init.TimeSeg2=CAN_BS2_7TQ;
hcan1.Init.Mode = CAN_MODE_NORMAL;
hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan1.Init.TimeTriggeredMode = DISABLE;
hcan1.Init.AutoBusOff = ENABLE;
hcan1.Init.AutoWakeUp = DISABLE;
hcan1.Init.AutoRetransmission = ENABLE;
hcan1.Init.ReceiveFifoLocked = DISABLE;
hcan1.Init.TransmitFifoPriority = DISABLE;
HAL_CAN_DeInit(&hcan1);
HAL_StatusTypeDef retval = HAL_CAN_Init(&hcan1);
HAL_CAN_Start(&hcan1);
HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING|CAN_IT_TX_MAILBOX_EMPTY);
}
The call of HAL_CAN_INIT(&hcan1) returns HAL_OK.
I try to send a message with:
void can_send_dummy_data(void){
//We send on ID 123, 4 Bytes: 0x3456789A
CAN_TxHeaderTypeDef tx_header;
tx_header.DLC=4;
tx_header.ExtId=0;
tx_header.StdId=0x123;
tx_header.IDE=CAN_ID_STD;
tx_header.RTR=CAN_RTR_DATA;
//Now data
uint8_t tx_data[4]={0x34,0x56,0x78,0x9A};
//Now send
uint32_t tx_mailbox;
HAL_StatusTypeDef retval=HAL_CAN_AddTxMessage(&hcan1,&tx_header,tx_data,&tx_mailbox);
}The retval ist also HAL_OK. But no message appears on the other side of the CAN Bus.
When I look into the
CAN_MSR:
0b0000 0000 0000 0000 0000 1100 0000 0000
RXM and TXM are set
CAN-TSR:
0b0001 1100 0000 0000 0000 0000 0000 0100
Transmit Mailbox 2 empty
Transmit Mailbox 1 empty
Transmit Mailbox 0 empty
Arbitration lost to mailbox 0
CAN-ESR
0b1000 0010 0000 0000 0000 0000 00010011
Receive error counter = 130 -> Error passive
LEC = Stuff Error
Error Passive flag
Error warning flag
So I have arbitration lost and stuff error and error passive.
If I exchange my Bluepill assembly by an STM8-Discovery-Board running a CAN Hello
world application on STM8, I can send CAN-Messages (500 kbit/s) without problem.
So I assume I made mistakes in my CAN initialization code on STM32.