STM32F3 UART Interrupt Bug
Hi, if I call: HAL_UART_Receive_IT, and I disable all the error IRQ (I don't want to be waken if I sleep) with the following instruction: __HAL_UART_DISABLE_IT(&huartx,UART_IT_ERR) ;
The uC stops to run because the HAL doesn't manage the IRQ error if they are disabled even if there are some pending interrupt so, inside the user code of the USARTx_IRQHandler() I have to put this code:
if((__HAL_UART_GET_IT(&huart1, UART_IT_FE) != RESET))
{
__HAL_UART_CLEAR_IT(&huart1, UART_CLEAR_FEF);
return;
}Is there a better solution?