STM32F334R8 ADC problem
Hello everyone!
I am trying to use the ADC of my NUCLEO-F334R8 board. I want to read the PC1 pin (ADC12, channel 7). I try to initialize the ADC with the following code:
void BSP_ADC_Init()
{
// Enable GPIOC clock
RCC->AHBENR |= RCC_AHBENR_GPIOCEN;
// Configure pin PC1 as analog
GPIOC->MODER &= ~GPIO_MODER_MODER1_Msk;
GPIOC->MODER |= (0x03 << GPIO_MODER_MODER1_Pos);
// Enable ADC clock
RCC->AHBENR |= RCC_AHBENR_ADC12EN;
// Reset ADC configuration
ADC1->CR = 0x00000000;
ADC1->CFGR = 0x00000000;
ADC1->SQR1 = 0x00000000;
// Enable continuous conversion mode
ADC1->CFGR |= ADC_CFGR_CONT;
// Select channel 7
ADC1->SQR1 |= (0x07 << ADC_SQR1_SQ1_Pos);
// Set sampling time to 19.5 ADC clock cycles
ADC1->SMPR1 = (0x04 << ADC_SMPR1_SMP7_Pos);
// 12-bit resolution
ADC1->CFGR |= (0x00 << ADC_CFGR_RES_Pos);
// Select PCLK/2 as ADC clock
RCC->CFGR2 |= (0x11 << RCC_CFGR2_ADCPRE12_Pos);
// Enable ADC
ADC1->CR |= ADC_CR_ADEN;
// Start conversion
ADC1->CR |= ADC_CR_ADSTART;
}
But it seems not to work. In the main, I get stuck in the loop:
// Wait here until ADC EOC
while ((ADC1->ISR & ADC_ISR_EOC) != ADC_ISR_EOC);
EOC never sets and DR is always 0.
Could anyone help me?