STM32F373 USB boot with 24MHz oscillator not crystal on HSE
I have 4 x STM32F373CCT6 on a custom board connected to a USB hub, all of which are clocked from a 3v3 24MHz oscillator ( rather than putting down 5 crystals and all the caps ). I have the 1k5 resistor pull up on the D+ line. when the board is powered up ( from the PC USB connection to the hub ) all 4 devices show as invalid descriptors when they enumerate
if i do a basic cube project setup with 24MHz bypass on the HSE and all the relevant clock setup, a CDC port enumerates fine when the device is programmed by either the UART or SWD connection so I know that the USB lines aren't the wrong way up , the clocks can be right inernally etc so fundamentally all can be ok but the DFU boot isn't
can someone point out the deliberate mistake?
thanks
Andy