STM32F401 ADC with DMA Example
I'm looking for an example to use as the starting point for a sensor data collector. In particular, an STM32F401 ADC_MultichannelSingleConversion with DMA and software start. I found an example for the F11 that is based on the LL SDK. I then created an F401 project using ADC with DMA and set the code generator to utilize the LL SDK for those components. I then compared the 'stm32f4xx_it' source and header files and found them substantially different. So much so, in fact, that I'm unsure how to proceed. The F11 example does not have an IOC file, so I cannot view its configuration settings. The code generated from my IOC file features very nice blocks that delineate where user code should be placed, and I want to utilize this feature to avoid conflicts with the code generator as I add other system components.
The same applies to the 'main' source and header files. If there's a better example to use as a starting point, or some guidance for merging the example code into a STM32Cube project, it would be really appreciated.