STM32F405 HAL I2C Code Bug Report
Code is missing:
typedef struct
{
__IO uint32_t CR1; /*!< I2C Control register 1, Address offset: 0x00 */
__IO uint32_t CR2; /*!< I2C Control register 2, Address offset: 0x04 */
__IO uint32_t OAR1; /*!< I2C Own address register 1, Address offset: 0x08 */
__IO uint32_t OAR2; /*!< I2C Own address register 2, Address offset: 0x0C */
__IO uint32_t DR; /*!< I2C Data register, Address offset: 0x10 */
__IO uint32_t SR1; /*!< I2C Status register 1, Address offset: 0x14 */
__IO uint32_t SR2; /*!< I2C Status register 2, Address offset: 0x18 */
__IO uint32_t CCR; /*!< I2C Clock control register, Address offset: 0x1C */
__IO uint32_t TRISE; /*!< I2C TRISE register, Address offset: 0x20 */
__IO uint32_t FLTR; /*!< I2C FLTR register, Address offset: 0x24 */ // Code is missing!
} I2C_TypeDef;
So, HAL_I2CEx_ConfigAnalogFilter() Function Occur Error:
if (hi2c->State == HAL_I2C_STATE_READY)
{
hi2c->State = HAL_I2C_STATE_BUSY;
/* Disable the selected I2C peripheral */
__HAL_I2C_DISABLE(hi2c);
/* Reset I2Cx ANOFF bit */
hi2c->Instance->FLTR &= ~(I2C_FLTR_ANOFF); // error: No Member
/* Disable the analog filter */
hi2c->Instance->FLTR |= AnalogFilter; // error: No Member
__HAL_I2C_ENABLE(hi2c);
hi2c->State = HAL_I2C_STATE_READY;
return HAL_OK;
}