Skip to main content
Graduate II
September 11, 2020
Question

stm32f407 USB HS CDC Problem

  • September 11, 2020
  • 0 replies
  • 571 views

hello everyone

Hello to everyone,

I have a project where I need to save data on a usb disk and communicate with the computer. I designed a circuit with a type A connector on the usb fs (a11 a12) line and a type b connector on the usb hs (b14 b15) line.

 usb fs line works in msc mode. I can write data to usb disk. but I could not run the usb hs line in cdc mode. I made a cdc example from usb fs line before. Anyone have any idea why the usb hs line is not working?

I'm using cubemx 6.0.1 and STM32Cube_FW_F4_V1.25.1.

I saw something like this while debugging. I did not set the usb to high speed operation. I seem to have connection with the problem.

0693W000003RRTkQAO.png

    This topic has been closed for replies.