STM32F407F4 Discovery: USART Master-Slave Communication Issue
I’m trying to establish USART communication between two STM32F407-Discovery boards, where one board acts as Master and the other as Slave.
Hardware setup
Master Board clk -> save board Clk - [common clock]
Master Board TX → Slave Board RX
Master Board RX ← Slave Board TX
Both GND connected
Using STM32F407-Discovery boards
SYNCHRONOUS MODE
connectivity configurations
USART port used (e.g., USART2)
Baud rate (e.g., 115200)
Word length (8 bits)
Parity (None)
Stop bits (1)
Clock settings ( synchronous)
clock polarity : low
clock phase : one edge
code of master and slave:// Master
char data = 'A';
HAL_USART_Transmit(&huart2, (uint8_t*)&data, 1, HAL_MAX_DELAY);// Slave
char rx;
HAL_USART_Receive(&huart2, (uint8_t*)&rx, 1, HAL_MAX_DELAY);output : Im getting grbage value like 127@ , so on
What I've tried
- Verified TX/RX wiring
- Checked baud rate matching
- Tried loopback test on each board (TX→RX)
- Switched from polling to interrupt-based reception