STM32F407G-Disc1 --> Controller Area Network receiver is not working in loopback mode
Hi Everyone,
i'm using two boards for my hobby purpose(stm32f108cxx bluepill board and stm32f407g discovery board). i tried the controller area network loopback mode in bluepill is working fine but in the stm32f407 discovery board controller area network is not working. For CAN transceiver i'm using sn65hvd230 IC. when absorb in the debugging mode transmitter is working fine but when pointer comes to receiver its not working. i pasted the code below
static void MX_CAN1_CONFIG(void)
{
CAN_FilterTypeDef can_filter;
can_filter.FilterActivation = CAN_FILTER_ENABLE;
can_filter.FilterBank = 0;
can_filter.FilterFIFOAssignment = CAN_FILTER_FIFO0;
can_filter.FilterIdHigh = 0x0000;
can_filter.FilterIdLow = 0x0000;
can_filter.FilterMaskIdLow = 0x0000;
can_filter.FilterMaskIdLow = 0x0000;
can_filter.FilterMode = CAN_FILTERMODE_IDMASK;
can_filter.FilterScale = CAN_FILTERSCALE_32BIT;
can_filter.SlaveStartFilterBank = 14;
if(HAL_CAN_ConfigFilter(&hcan1, &can_filter) != HAL_OK)
{
Error_Handler();
}
if(HAL_UART_Transmit(&huart2,(uint8_t *)msg[2], strlen(msg[2]), 10) != HAL_OK)
{
Error_Handler();
}
}
static void MX_CAN1_TX(void)
{
CAN_TxHeaderTypeDef Tx_Handler;
uint8_t tmsg[] = "Hello";
uint32_t TxMailbox;
Tx_Handler.DLC = 8;
Tx_Handler.ExtId = 0;
Tx_Handler.IDE = CAN_ID_STD;
Tx_Handler.RTR = CAN_RTR_DATA;
Tx_Handler.StdId = 0x65d;
Tx_Handler.TransmitGlobalTime = DISABLE;
if(HAL_CAN_AddTxMessage(&hcan1, &Tx_Handler, tmsg,&TxMailbox ) != HAL_OK)
{
Error_Handler();
}
while(HAL_CAN_IsTxMessagePending(&hcan1, TxMailbox));
if(HAL_UART_Transmit(&huart2,(uint8_t *)msg[3], strlen(msg[3]), 10) != HAL_OK)
{
Error_Handler();
}
}
static void MX_CAN1_RX(void)
{
CAN_RxHeaderTypeDef can_rxheader;
uint8_t rx_data[5];
while(!HAL_CAN_GetRxFifoFillLevel(&hcan1, CAN_FILTER_FIFO0));
if(HAL_CAN_GetRxMessage(&hcan1,CAN_FILTER_FIFO0,&can_rxheader, rx_data) != HAL_OK)
{
Error_Handler();
}
if(HAL_UART_Transmit(&huart2,(uint8_t *)msg[4], strlen(msg[4]), 10) != HAL_OK)
{
Error_Handler();
}
}
code is stuck in the receiver section
"while(!HAL_CAN_GetRxFifoFillLevel(&hcan1, CAN_FILTER_FIFO0));"