STM32F407VGT7 I use system memory boot mode by USART1 (PA10, PA9). i have to use external pull-up/pull-down resistors to USART3 (PB10 / PB11, PC10 / PC11), CAN2 (PB5), USB (PA11, PA12)?
STM32F407VGT7
I use system memory boot mode by USART1 (PA10, PA9). i have to use external pull-up/pull-down resistors to USART3 (PB10 / PB11, PC10 / PC11), CAN2 (PB5), USB (PA11, PA12)?
PA10, PA9 connect to external pull-up resistors 7.5Kohms.
If don't connect resistors, will there be programming problems?
My project use pin PA11 - exit. PA11 connect to bus transceiver SN74LVC2T45. no external pull-up/pull-down resistors.