STM32F412 HardFault_Handler while trying to create new file system
Dear ST Community, Dear ST Team.
To implement a small USB Device i working with STM32F412 MCU and a Flash Chip mt25ql512.
The Good Part is, that the QSPI Communication works absolutly fine and i can read, write the flash and erase the Chip.
Next Step is to Implement a small Filesystem with FATFS.
After the Standard settings and configure the user_diskio.c, i stuck in the HardFault_Handler after the call f_mkfs() function. So im sitting on a dead end and im glad to hear some ideas or information about that topic.
Thanks for your help.
Thx RSheetz
/********************************************************************************************/
void FatFS_USB_init(void)
{
// FATFS_LinkDriver(&Flash_Driver, USERPath);
FRESULT res = f_mount(&USERFatFS, USERPath, 1);
// If FatFS fails mounting process, create new file system
if (res != FR_OK)
{
f_mkfs(USERPath, FM_FAT32, 0, workBuffer, sizeof(workBuffer));
res = f_mount(&USERFatFS, USERPath, 1);
}
}
/********************************************************************************************/
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file user_diskio.c
* @brief This file includes a diskio driver skeleton to be completed by the user.
******************************************************************************
* @attention
*
* Copyright (c) 2025 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
#ifdef USE_OBSOLETE_USER_CODE_SECTION_0
/*
* Warning: the user section 0 is no more in use (starting from CubeMx version 4.16.0)
* To be suppressed in the future.
* Kept to ensure backward compatibility with previous CubeMx versions when
* migrating projects.
* User code previously added there should be copied in the new user sections before
* the section contents can be deleted.
*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
#endif
/* USER CODE BEGIN DECL */
/* Includes ------------------------------------------------------------------*/
#include <string.h>
#include "ff_gen_drv.h"
#include "qspiFlashHandler.h"
#include "mt25ql512.h"
/* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*/
/* Private variables ---------------------------------------------------------*/
/* Disk status */
static volatile DSTATUS Stat = STA_NOINIT;
/* USER CODE END DECL */
/* Private function prototypes -----------------------------------------------*/
DSTATUS USER_initialize (BYTE pdrv);
DSTATUS USER_status (BYTE pdrv);
DRESULT USER_read (BYTE pdrv, BYTE *buff, DWORD sector, UINT count);
#if _USE_WRITE == 1
DRESULT USER_write (BYTE pdrv, const BYTE *buff, DWORD sector, UINT count);
#endif /* _USE_WRITE == 1 */
#if _USE_IOCTL == 1
DRESULT USER_ioctl (BYTE pdrv, BYTE cmd, void *buff);
#endif /* _USE_IOCTL == 1 */
Diskio_drvTypeDef USER_Driver =
{
USER_initialize,
USER_status,
USER_read,
#if _USE_WRITE
USER_write,
#endif /* _USE_WRITE == 1 */
#if _USE_IOCTL == 1
USER_ioctl,
#endif /* _USE_IOCTL == 1 */
};
/* Private functions ---------------------------------------------------------*/
/**
* @brief Initializes a Drive
* @PAram pdrv: Physical drive number (0..)
* @retval DSTATUS: Operation status
*/
DSTATUS USER_initialize (
BYTE pdrv /* Physical drive nmuber to identify the drive */
)
{
/* USER CODE BEGIN INIT */
Stat = STA_NOINIT;
if (pdrv != 0)
{
return STA_NOINIT;
}
Stat = QSPIFL_init(); // QSPIFL_init(); needs to run before
return RES_OK;
/* USER CODE END INIT */
}
/**
* @brief Gets Disk Status
* @PAram pdrv: Physical drive number (0..)
* @retval DSTATUS: Operation status
*/
DSTATUS USER_status (
BYTE pdrv /* Physical drive number to identify the drive */
)
{
/* USER CODE BEGIN STATUS */
Stat = STA_NOINIT;
return Stat;
/* USER CODE END STATUS */
}
/**
* @brief Reads Sector(s)
* @PAram pdrv: Physical drive number (0..)
* @PAram *buff: Data buffer to store read data
* @PAram sector: Sector address (LBA)
* @PAram count: Number of sectors to read (1..128)
* @retval DRESULT: Operation result
*/
DRESULT USER_read (
BYTE pdrv, /* Physical drive nmuber to identify the drive */
BYTE *buff, /* Data buffer to store read data */
DWORD sector, /* Sector address in LBA */
UINT count /* Number of sectors to read */
)
{
/* USER CODE BEGIN READ */
if (pdrv != 0 || Stat & STA_NOINIT)
{
return RES_NOTRDY;
}
uint32_t addr = sector * MT25QL512_MEMORY_SECTOR_SIZE;
uint32_t size = count * MT25QL512_MEMORY_SECTOR_SIZE;
if (QSPIFL_readMemory(buff, addr, size) != QSPIFL_OK)
{
return RES_ERROR;
}
return RES_OK;
/* USER CODE END READ */
}
/**
* @brief Writes Sector(s)
* @PAram pdrv: Physical drive number (0..)
* @PAram *buff: Data to be written
* @PAram sector: Sector address (LBA)
* @PAram count: Number of sectors to write (1..128)
* @retval DRESULT: Operation result
*/
#if _USE_WRITE == 1
DRESULT USER_write (
BYTE pdrv, /* Physical drive nmuber to identify the drive */
const BYTE *buff, /* Data to be written */
DWORD sector, /* Sector address in LBA */
UINT count /* Number of sectors to write */
)
{
/* USER CODE BEGIN WRITE */
/* USER CODE HERE */
if (pdrv != 0 || Stat & STA_NOINIT)
{
return RES_NOTRDY;
}
uint32_t addr = sector * MT25QL512_MEMORY_SECTOR_SIZE;
uint32_t size = count * MT25QL512_MEMORY_SECTOR_SIZE;
if (QSPIFL_eraseSector(addr, addr + size) != QSPIFL_OK)
{
return RES_ERROR;
}
if (QSPIFL_writeMemory((uint8_t *)buff, addr, size) != QSPIFL_OK)
{
return RES_ERROR;
}
return RES_OK;
/* USER CODE END WRITE */
}
#endif /* _USE_WRITE == 1 */
/**
* @brief I/O control operation
* @PAram pdrv: Physical drive number (0..)
* @PAram cmd: Control code
* @PAram *buff: Buffer to send/receive control data
* @retval DRESULT: Operation result
*/
#if _USE_IOCTL == 1
DRESULT USER_ioctl (
BYTE pdrv, /* Physical drive nmuber (0..) */
BYTE cmd, /* Control code */
void *buff /* Buffer to send/receive control data */
)
{
/* USER CODE BEGIN IOCTL */
DRESULT res = RES_ERROR;
return res;
/* USER CODE END IOCTL */
}
#endif /* _USE_IOCTL == 1 */