STM32F429 RTOS and SD card
I have a application with STM32F429 with RTOS and SPI µSD .
I have a singke task forr write in SD card and some time goes in HardFault_Handler ()
It is possible thei is caused by stack overflow ?
How can I check if the stack pointer goes in overflow ?
Thanks
#define configMINIMAL_STACK_SIZE ((uint16_t)128)
osThreadDef(sD_Task, SD_Task, osPriorityNormal, 0, configMINIMAL_STACK_SIZE);
.........................
void SD_Task(void const * argument)
{
while(1) {
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_12,GPIO_PIN_SET); // debugga LED AUX2
update_file_log("NEW LOG \r\n", 22);
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_12,GPIO_PIN_RESET); // debugga LED AUX2
// HAL_GPIO_TogglePin(LD3_GPIO_Port, LD3_Pin);
osDelay(1000);
}
}
static uint8_t update_file_log(char * folder, char* s, int lunghezza)
{ uint8_t log_esiste=0;
uint8_t return_value =1;
BYTE writeBuf[256];
uint16_t st;
st = HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_15); // insert pin
if ( st == 1) {
fres = f_mount(&FatFs, "", 1); //1=mount now
if (fres == FR_OK) {
DWORD free_clusters;
FATFS* getFreeFs;
fres = f_getfree("", &free_clusters, &getFreeFs);
if (fres == FR_OK) {
fres = f_opendir (&dp, folder);
if (fres != FR_OK) {
f_mkdir (folder);
}
f_chdir (folder);
fres = f_open(&fil, FILE_LOG_NAME, FA_READ);
if (fres == FR_OK) {
log_esiste =1;
f_close(&fil);
}
if (log_esiste==0) {
fres = f_open(&fil, FILE_LOG_NAME, FA_WRITE | FA_OPEN_ALWAYS | FA_CREATE_ALWAYS);
} else {
fres = f_open(&fil, FILE_LOG_NAME, FA_WRITE | FA_OPEN_APPEND );
}
if (fres == FR_OK) {
strncpy((char*)writeBuf, s, lunghezza);
UINT bytesWrote;
fres = f_write(&fil, writeBuf, lunghezza, &bytesWrote);
f_close(&fil);
return_value = 0;
}
}
}
f_mount(NULL, "", 0);
}
return return_value;
}