STM32F723 USBPHYC LDO control documentation/HAL bug
So I'm looking at the reference manual of STM32F723 to find out how to control the USBPHYC peripheral. Actually there is no programmer's guide in there like for most peripherals, so I can only rely on the register map to find anything out about it. The LDO register has an LDO_DISABLE bit, that shall be set to 1 to disable the LDO.
Now let's check the HAL drivers:
stm32f7xx_ll_usb.c has USB_HS_PHYCInit() function to start the PHYC (but there's no function to stop it...). The first step of this function is:
/* Enable LDO */
USB_HS_PHYC->USB_HS_PHYC_LDO |= USB_HS_PHYC_LDO_ENABLE;Well that's strange, I didn't find an LDO_ENABLE bit in the reference manual. But when I look at this definition, turns out:
/* Legacy */
[...]
#define USB_HS_PHYC_LDO_ENABLE USB_HS_PHYC_LDO_DISABLESo this is confusing. To "Enable LDO", one must set the DISABLE bit? There must be an error in either the HAL drivers or in the reference manual (+ the CMSIS header of the devices). The question is, which one is the incorrect one? And when will it get fixed?