Skip to main content
Visitor II
October 24, 2024
Solved

STM32F746 Flash Sector Erase Problem

  • October 24, 2024
  • 2 replies
  • 907 views

Hi Guys,

I have a problem with erasing Flash sector. I am using STM32F746ZG Nucleo Board. When  I run this code, mcu works perfect it works but I can't install new firmware to mcu. I've also tried example code, same problem. I take (DEV_TARGET_NOT_HALTED) when I run the program.

I am getting the same error in debug mode as described in the link below.

https://community.st.com/t5/stm32cubeide-mcus/how-to-solve-error-finishing-flash-operation-in-stm32cubeide/td-p/53113/page/2

Code Here they are

 

FLASH_EraseInitTypeDef FLASH_Erase_Init;
uint32_t SectorError;

HAL_FLASH_Unlock();

FLASH_Erase_Init.TypeErase = FLASH_TYPEERASE_SECTORS;
FLASH_Erase_Init.VoltageRange = FLASH_VOLTAGE_RANGE_3;
FLASH_Erase_Init.Sector. FLASH_SECTOR_3;
FLASH_Erase_Init.NbSectors = 1;

if(HAL_FLASHEx_Erase(&FLASH_Erase_Init, &SectorError) == HAL_OK)
HAL_Flash_Lock();

 

 

How can i solve it ?

    This topic has been closed for replies.
    Best answer by BahadirA

    I've solved this issue with changing Reset Behaviour from Connect under reset to None.

    2 replies

    ST Employee
    October 24, 2024

    Hello @BahadirA ,

    Please refer to the reference manual RM0385 / Table 3. STM32F756xx and STM32F74xxx Flash memory organization of how the sectors are organized.

    For erase_init.Sector and erase_init.NbSectors parameters, I propose to follow this example. These two parameters are provided by GetSector().

     FirstSector = GetSector(FLASH_USER_START_ADDR);
     /* Get the number of sector to erase from 1st sector*/
     NbOfSectors = GetSector(FLASH_USER_END_ADDR) - FirstSector + 1;
     /* Fill EraseInit structure*/
     EraseInitStruct.TypeErase = FLASH_TYPEERASE_SECTORS;
     EraseInitStruct.VoltageRange = FLASH_VOLTAGE_RANGE_3;
     EraseInitStruct.Sector = FirstSector;
     EraseInitStruct.NbSectors = NbOfSectors;
    

    PS: you can also to refer to AN4657 "STM32 in-application programming (IAP) using the USART" for a customized bootloader via UART.

    Regards.

    BahadirAAuthorAnswer
    Visitor II
    October 25, 2024

    I've solved this issue with changing Reset Behaviour from Connect under reset to None.