stm32f746 uclinux kernel build toolchain
hi,
i'm trying to build the kernel source on the stm32f746-disco
i'have forked github link of kernel source
https://github.com/KpuFish/linux-stm32f7
regarding the step discriptions,
-->>
Steps to make the uImage :
1) use `make stm32f746_disco_defconfig' to configure a kernel configuration with
support following STM32 IPs: USART, LTDC (framebuffer).
2) `sudo tar xf initdir.tar', to extract initdir.tar to initdir directory.
Note: use `sudo' to ensure `tar' will succesfull create dev nodes.
3) `export ARCH=arm'
4) `export CROSS_COMPILE=arm-uclinuxeabi-'
Note: arm-uclinuxeabi-* toolchain may be in your path.
Note: arm-uclinuxeabi- toolchain provided by sourcery in link[1]
5) `make', to compile kernel
6) to create loadable uImage:
`mkimage -A arm -a 0xc0008000 -e 0xc0008001 -n 'Linux kernel0' -C none -T kernel -d arch/arm/boot/Image networking.uImage'
i'm stuck in step (5)
i have tried many times set the PATH commands
although i also have modified bashrc same thing, it failed to build current source and not created uImage file
i think the path setting is something worng.
but i don't know what is worng
i've added path below in bashrc
export PATH=/home/djpark/downloads/stm32f746-disco_linux-master/arm-2011.03/bin:$PATH
export CROSS_COMPILE=arm-uclinuxeabi-
export ARCH=arm
and real path of...
stm32f746 source is /home/djpark/downloads/stm32f746-disco_linux
and uclinux toolchain is
/home/djpark/downloads/stm32f746-disco_linux/arm-2011.03
when i try to build using make command, it is failed.
it means just no such files or directory ...
am i worng?