[STM32F767] Shift occurs when reading NAND memory data.
Dear all
nand memory device is MT29F4G. I attacing datasheet
first nand memory setting.
===========================================================
hnand1.Instance = FMC_NAND_DEVICE;
/* hnand1.Init */
hnand1.Init.NandBank = FMC_NAND_BANK3;
hnand1.Init.Waitfeature = FMC_NAND_WAIT_FEATURE_ENABLE;
hnand1.Init.MemoryDataWidth = FMC_NAND_MEM_BUS_WIDTH_8;
hnand1.Init.EccComputation = FMC_NAND_ECC_ENABLE;
hnand1.Init.ECCPageSize = FMC_NAND_ECC_PAGE_SIZE_2048BYTE;
hnand1.Init.TCLRSetupTime = 0;
hnand1.Init.TARSetupTime = 0;
/* hnand1.Config */
hnand1.Config.PageSize = 2048;
hnand1.Config.SpareAreaSize = 64;
hnand1.Config.BlockSize = 64;
hnand1.Config.BlockNbr = 2048;
hnand1.Config.PlaneNbr = 2;
hnand1.Config.PlaneSize = 2048;
hnand1.Config.ExtraCommandEnable = DISABLE;
/* ComSpaceTiming */
ComSpaceTiming.SetupTime = 5;
ComSpaceTiming.WaitSetupTime = 5;
ComSpaceTiming.HoldSetupTime = 6;
ComSpaceTiming.HiZSetupTime = 0;
/* AttSpaceTiming */
AttSpaceTiming.SetupTime = 5;
AttSpaceTiming.WaitSetupTime = 5;
AttSpaceTiming.HoldSetupTime = 6;
AttSpaceTiming.HiZSetupTime = 0;
============================================================
when I read NAND nomal: 
When I read Nand , data is shift
HAL_NAND_Read_Page_8b source :
=====================================================================
{
*(__IO uint8_t *)((uint32_t)(deviceAddress | ADDR_AREA)) = 0x00;
__DSB();
*(__IO uint8_t *)((uint32_t)(deviceAddress | ADDR_AREA)) = 0x00;
__DSB();
*(__IO uint8_t *)((uint32_t)(deviceAddress | ADDR_AREA)) = Third_Address;//ADDR_1ST_CYCLE(nandAddress);
__DSB();
*(__IO uint8_t *)((uint32_t)(deviceAddress | ADDR_AREA)) = Fourth_Address;//ADDR_2ND_CYCLE(nandAddress);
__DSB();
*(__IO uint8_t *)((uint32_t)(deviceAddress | ADDR_AREA)) = Fifth_Address;//ADDR_3RD_CYCLE(nandAddress);
__DSB();
}
}
*(__IO uint8_t *)((uint32_t)(deviceAddress | CMD_AREA)) = NAND_CMD_AREA_TRUE1;
__DSB();
for(; index < size; index++)
{
*(uint8_t *)pBuffer++ = *(uint8_t *)deviceAddress;
}
=========================================================================
when I test on ST32F407 , it is working well.
But when I test on ST32F767 , data is shift.
Let me know why this is happening.
Thanks.