STM32F769 ST Bootloader
Dear,
I have an issue about the embedded ST bootloader on the STM32F769. I'm not able to communicate with it.
On a custom board, I use a STM32F769BG connected to the USART 1 (PA9 / PA10). When I send the 0x7F value, I don't have a response from the MCU. The startup step is follow :
- low state on the RST pin and BOOT 0 pin (MCU in reset state)
- high state on BOOT 0 pin
- wait 5 ms for pin state stabilization
- high state on RST pin
- wait 5 ms for pin state stabilization
- sending 0x7F value
I also try with the STM32F7 discovery (https://www.st.com/en/evaluation-tools/32f769idiscovery.html) but I have the same issue. On this board, I have unsolder the resistors between the MCU and the embedded ST-Link because it's the USART 1 which is used to do it.
I'm sure that it's not my custom application which is launch when I release the RST pin, because I did a led blinker firmware and when I did the previous step to entre the MCU into the ST bootloader, the led don't blink.
I already used this step to update other MCU (STM32F030RC and STM32F072C8) and it working well.
Maybe I missing something or doing something wrong ?