STM32F769I USB-HS MSC gives low read/write speed
Hi,
I am using a STM32F769I Disco board for testing the speeds of the High Speed USB as a MSC. At present, the system is working as expected as a MSC over uSD. However, my concern is with respect to the read write speed of 2.5MB/s which seems to be very low for High Speed Applications. I have used the HAL Libraries and ST provided Examples for the firmware.
At the uSD side, I am able to get a speed of 6 MB/s, but when the read write is over HS-USB as MSC, the speed I get is around 2.5MB/s.
Would be very helpful if any one can provide any insights.
Thank You,
Amit K