Skip to main content
Visitor II
December 29, 2024
Question

STM32G030 and X-CUBE-EEPROM

  • December 29, 2024
  • 0 replies
  • 611 views

Hi, I'm trying to use https://www.st.com/en/embedded-software/x-cube-eeprom.html on my custom stm32g030 board.

Following the examples I write this code:

 

 

 HAL_FLASH_Unlock();

 ee_status = EE_Init(EE_FORCED_ERASE);
 if(ee_status != EE_OK) {
	 Error_Handler();
 }


 VarValue = 3;
 for (Index = 1; Index < NB_OF_VARIABLES+1; Index++)
 {
	 ee_status = EE_WriteVariable32bits(Index, Index*VarValue);
	 /* Start cleanup polling mode, if cleanup is needed */
	 if ((ee_status & EE_STATUSMASK_CLEANUP) == EE_STATUSMASK_CLEANUP) {ErasingOnGoing = 0;ee_status|= EE_CleanUp();}
	 if ((ee_status & EE_STATUSMASK_ERROR) == EE_STATUSMASK_ERROR) {Error_Handler();}
 }

 for (uint8_t idx = 0; idx < NB_OF_VARIABLES; idx++)
 {
	 // Virtual address arranca en 1
	 ee_status = EE_ReadVariable32bits(idx+1, &VarValue);
	 if (ee_status != EE_OK) {Error_Handler();}
 }

 /* Lock the Flash Program Erase controller */
 HAL_FLASH_Lock();

 

 

I unlock the flash, the Init the EE emulation, write 10 variables (check if a cleanup is required), then read back the values.

This works ok. After running this code a couple of time I get:

Lgarb1_0-1735511572087.png

I'm not sure why I have 4*32 bits with 0xFFFFFFFF on 0x08007810.

Then I get 16 bits VA (0001) 16 bits CRC (80E01) and 32 bits value 00000003.

Then I want to try to read data after power off. So I comment back writing operations, flash the code and connect with STM32 Programmer to read the data. I get the following:

Lgarb1_1-1735512281721.png

each time I re-connect the programmer (and so a reset is made) 2x32 bits 0's are written into the flash. It's come from ee_status = EE_Init(EE_FORCED_ERASE); calling that is forcing the write of those 0's. I've tried with EE_CONDITIONAL_ERASE but the same happens.

My configuration is as follow:

 

 

/* Configuration of eeprom emulation in flash, can be custom */
#define START_PAGE_ADDRESS (FLASH_BASE + (14 * FLASH_PAGE_SIZE)) //0x08080000U /*!< Start address of the 1st page in flash, for EEPROM emulation */
#define CYCLES_NUMBER 1U /*!< Number of 10Kcycles requested, minimum 1 for 10Kcycles (default),
 for instance 10 to reach 100Kcycles. This factor will increase
 pages number */
#define GUARD_PAGES_NUMBER 0U /*!< Number of guard pages avoiding frequent transfers (must be multiple of 2): 0,2,4.. */

/* Configuration of crc calculation for eeprom emulation in flash */
#define CRC_POLYNOMIAL_LENGTH LL_CRC_POLYLENGTH_16B /* CRC polynomial lenght 16 bits */
#define CRC_POLYNOMIAL_VALUE 0x8005U /* Polynomial to use for CRC calculation */

 

 

Any help will be appreciated.

    This topic has been closed for replies.