Skip to main content
Visitor II
November 6, 2023
Question

STM32G030 sometimes not waking up from STOP 1 Mode

  • November 6, 2023
  • 1 reply
  • 1788 views

Hey everyone, I have developed a circuit board with STM32G030. I use the STOP 1 mode to save power, the device wakes up on a pin change interrupt.

Sometimes the current consumption in STOP 1 mode is around 1,2mA higher mode than normal (3uA) but lower than run mode(2,5mA) and the MCU does not wake up anymore. The same in Standby Mode.

I can´t find the reason, maybe someone has an idea.

 

Here is my STOP Mode function:

void StopMode(void)

{

LED_On(OFF);

I2C_On(OFF);

MOT_EN(OFF);

//DisableDebugger();

//disablePeripherie();

HAL_SuspendTick();

sleep = 1;

HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI); //Stop 1

 

SystemClock_Config();

HAL_ResumeTick();

 

USR_LED_On(1);

 

LED_On(ON);

I2C_On(ON);

MOT_EN(ON);

}

    This topic has been closed for replies.

    1 reply

    JakobBAuthor
    Visitor II
    November 6, 2023

    After some testing I figured out that the problem is only present when I run the Timer 3 with PWM generation before going to sleep. The Errata sheet mentions something but my HSI_DIV is set to [00]

    code out of main.c:

    RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;

     

    STM32G030x6/x8 device errata:

    2.2.6 Wakeup from Stop not effective under certain conditions
    Description
    With the HSI clock divider bitfield HSIDIV[2:0] set to a value different from 000, the device fails to enter Stop
    mode when SYSCLK is set to HSE clock.
    With the HSI clock divider bitfield HSIDIV[2:0] set to a value different from 000, peripherals with clock request
    capability fail to wake the device up from Stop modes.
    Workaround
    None.

    Visitor II
    February 27, 2024

    Hello JakobB,

     

    could you figure out your problem ?

    We have a similar issue using an STM32G0B1 ...

     

    Best regards,

    lakeroe