STM32G031 Interrupts not working after jump from IAP
Hi all
I am working with STM32G031F4 on a custom board and using STM32CubeIDE.
I have a small bootloader that jumps to the application after some time (based on HAL_GetTick()), but none of the interrupts seems to be running after the jump- namely UART and SysTick are of interest.
I have tried
int main(void)
{
SCB->VTOR=0x08001000;
...as I have same approach on STM32F407 (where it works)
I have also tried mapping the vector table to the beginning of the ram
int main(void)
{
/* USER CODE BEGIN 1 */
for(uint32_t i = 0; i < 48; i++)
{
VectorTable[i] = *(__IO uint32_t*)(APPLICATION_ADDRESS + (i<<2));
}
/* Remap SRAM at 0x00000000 */
__HAL_RCC_SYSCFG_CLK_ENABLE();
LL_SYSCFG_SetRemapMemory(LL_SYSCFG_REMAP_SRAM);
....which was suggested somewhere on this forum for the Cortex-M0.
When I omit the BL and load the APP from the beginning of the flash it works fine (with commenting the change to VTOR)
I have also tried the simple bootloader/blinky app for the STM32G031 Nucleo-32 board with no success.
And interestingly (at least for me), if I run the app using the debugger, it works just fine (on both boards)
Any ideas what I might be missing?
Thanks in advance