STM32G0B1KBU USB-C CC2
Im looking to use the STM32G0B1KBU processor including the USB-C interface.
I only want to use it as a UPF with VCP and update the firmware, no advanced PD or role switching.
The issue is that UCPD1_CC2 is not routed to a pin on the processor.
Is it possible to substitute the UCPD1_CC2 function with the "Dead battery pulldowns" UCPD1_DBCC2?
Will it work with the bootloader after the "dead battery" has been programmed/configured?
I could place the CC1 & CC2 pulldowns discreetly on the board but i am space constrained.
I could also switch to the N variant of the processor that seems to have the UCPD1_CC2 pin broken out. I Already have several of the GP variants laying around from a previous project and want to reuse them if possible.
Thanks for any input!