Skip to main content
Visitor II
August 11, 2022
Question

stm32g0b1ke mcu i2c not detected after flashing into flash memory

  • August 11, 2022
  • 0 replies
  • 483 views

I have flashed the firmware into flash memory using i2c application programming.when the controller is booting from flash memory,i can see the uart console logs .

I have configured the PB6 and PB7 pins are i2c pins.I set the clock speed to fast mode using stm32cubemx generator.I2c own address bit also set with 7bit I2C address << 1.But i2c is not detected.Is there any configuration missing?

    This topic has been closed for replies.