Question
STM32G4 ADC12_Common Register cannot be written
Hi! I am trying to set ADC pre-scaler of my STM32G431KB however no matter what I do it never changes from 0x0.
I can setup ADC1 register without a problem but when it comes to ADC12_Common register nothing seems to be configurable.
Below there is my ADC configuration code.
//-------------ADC Configuration-------------//
ADC1->CR &= ~(ADC_CR_ADEN); //Disable ADC
ADC12_COMMON->CCR |= (0b00<<ADC_CCR_CKMODE_Pos); //Select ADC clock Source in Peripheral
ADC12_COMMON->CCR |= (0b1000<<ADC_CCR_PRESC_Pos); //ADC Clock divided by 32
ADC1->CR &= ~(ADC_CR_DEEPPWD); //Disable ADC Deep-Power-Down mode
ADC1->CR |= ADC_CR_ADVREGEN; //Enable ADC Voltage Regulator
DummyDelay(10000); //Delay for ADC Voltage regulator settling
ADC1->CFGR |= ADC_CFGR_CONT; //ADC continuous mode
ADC1->CFGR &= ~(ADC_CFGR_RES); //12-bit ADC
ADC1->SQR1 |= (0b0000 << ADC_SQR1_L_Pos) | (1 << ADC_SQR1_SQ1_Pos); // Only 1 conversion for ADC channel 1
ADC1->DIFSEL &= ~(ADC_DIFSEL_DIFSEL_0); //Single Ended Input
ADC1->CFGR2 |= (0b0001 << ADC_CFGR2_OVSS_Pos); //Over-sampling mode 1 bit shift
ADC1->CFGR2 |= (0b001 << ADC_CFGR2_OVSR_Pos); //Over-sampling ratio x4
ADC1->CFGR2 |= ADC_CFGR2_ROVSE; //Enable Over-sampling
ADC1->CFGR |= ADC_CFGR_DMAEN | ADC_CFGR_DMACFG; //Enable DMA for ADC and DMA in Circular Mode
ADC1->CR &= ~(ADC_CR_ADCALDIF); //Single Ended Mode Calibration
ADC1->CR |= ADC_CR_ADCAL; //Start Calibration
while(ADC1->CR & ADC_CR_ADCAL); //Wait Until Calibration Complete
ADC1->ISR |= ADC_ISR_ADRDY; //Clear ADRDY Flag
ADC1->CR |= ADC_CR_ADEN; //Enable ADC
while(!(ADC1->ISR & ADC_ISR_ADRDY)); //Wait Until ADC EnablesCan someone tell me what I am doing wrong in line 3 and 4 of above code?