STM32G474 jump to ST Bootloader without Boot0 pin
Hi,
I'm trying to boot to the system memory so I could use ST bootloader (USB-DFU in mind), but unfortunately not succeeded.
I have a custom board with a STM32G474RE and another similar version with a STM32G473RB. I cannot use the PB8/Boot0 pin, cause I am using the pin for the CAN_RX with a MCP2562 chip. I have the Option Bytes as follow:
BFB2 = 0, nBOOT1 = 1, nSWBOOT0 = 0, nBOOT0 = 0, BOOT_LOCK = 0
This is what is written in the STM32G4 Manual to disable PB8 and make a sw jump to the bootloader but doesn't work.
I also have tried to boot (at the addr.: 0x1FFF0000) directly from the main(), with the function below:
__attribute__((naked, noreturn)) void BootJumpASM(uint32_t SP, uint32_t RH)
{
__asm("MSR MSP,r0");
__asm("BX r1");
}
void bl_flash_jump_to_address(uint32_t address)
{
/* BootJump done as explained by ARM documentation */
/* Disable SysTick and clear its exception pending bit */
SysTick->CTRL = 0;
SCB->ICSR |= SCB_ICSR_PENDSTCLR_Msk;
/* Disable individual fault handlers */
// not necessary here (?)
/* Activate the MSP, if the core is
* found to currently run with the PSP */
if (CONTROL_SPSEL_Msk & __get_CONTROL())
{/* MSP is not active */
__set_MSP(__get_PSP());
__set_CONTROL(__get_CONTROL() & ~CONTROL_SPSEL_Msk);
}
/* Load the vector table address of the user application */
SCB->VTOR = address;
/* Set the MSP to the value in user application VTOR
* and then load the PC with the reset vector value
* of the user application */
BootJumpASM(*(volatile uint32_t*) address,
*(volatile uint32_t*) (address + 4U));
}
int main(void)
{
__disable_irq();
SYSCFG->MEMRMP = 0x01; // 0x0000 0000 map to system memory
bl_flash_jump_to_address(0x1FFF0000) // address of the system memory
}Some observations:
1- The USB on my custom board and the board itself works fine. I can run my applications on it and all peripherals (UART, SPI, GPIO, HSE, ADC, DAC etc). I can set USB-CDC or I can also set USB-DFU generated by CubeMX with no problem.
2- The code to make the jump works, because I can make the jump to my app (ie. address 0x8008000)
3 - The board is powered by USB 5V and converted to 3V3, that goes to all the VDD & VBAT pins
4 - I have a Nucleo Board STM32G474, I tested with the Option Bytes, and with the code above. I can jump to the ST Bootloader with no issue - which makes me more confuse.
Am I am missing something or can it be a Hardware issue on my custom board?
Thanks