STM32G474RE opamps bias
Hello,
I am thinking of buying an nucleo-g474re for 3-channel DMA sampling from the ADCs. Before I acquire one, I'd like to know if it can fit my use case. There are three analog input sources. Each one ranges from -100mV to +100mV. Is it possible for me to use 3 opamp pins to offset the negative voltages to positive and subsequently amplify to 3.3V? I know it is possible to use the DAC to set the input voltage offset with at least one pin, but I would like to know if this can be done for three. Once I offset, can I route directly to the ADC pins? Can I do this all internally, with no external wires, resistors, and boards?
Thank you for your help