STM32G491 bootloader doesn't work
hi, i'm using a STM32G491 and i can't use embedded bootloader over UART1.
i'v set BOOT_LOCK(bit) to 0, Boot0(pin) to 1, nBoot1(bit) to 1 ans nBoot_SW(bit) to 1.
when i try to connect the mcu to STCubeProgrammer over UART i receive this message error:
17:18:05:955 : Serial Port COM7 is successfully opened.
17:18:05:955 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off
17:18:05:955 : No Init bits value is : 0
17:18:05:955 : Sending init command:
17:18:05:957 : byte 0x7F sent successfully to target
17:18:07:956 : Wait ends after 1 loop, dataready = 0, delay = 2001
17:18:07:956 : Timeout error occured while waiting for acknowledgement.
17:18:07:956 : No response from target received
17:18:07:957 : byte 0x7F sent successfully to target
17:18:08:056 : Wait ends after 1 loop, dataready = 0, delay = 100
17:18:08:056 : Timeout error occured while waiting for acknowledgement.
17:18:08:056 : No response from target received
17:18:08:056 : Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again...
17:18:08:128 : UART PORT CLOSE
someone can help me?