Skip to main content
Visitor II
December 11, 2024
Solved

STM32H5 self-test library DSP-support enabled

  • December 11, 2024
  • 1 reply
  • 861 views

I use a STM32H5 with STM32_Safety_STL v4.0.0 library. Development tool IAR 9.60.3

Using the project NUCLEO-H563ZI without TrustZone in X-CUBE-CLASSB-H5 and compiling it, I have the following linker error:

"Error[Lt069]: The module stl_sch_main.o(STL_Lib.a) (and 13 more) has DSP-support enabled, but the current CPU does not."

SOLVED enabling option on 32bit tab: "DSP extension"

 

    This topic has been closed for replies.
    Best answer by STea

    Hello @FPasq.1 ,

    If I get you correctly you managed to solve the issue by enabling the DSP extension. if it is the case or you have more details, we can close the thread by marking a reply as solution for better visibility to other uses.
    Regards 

    1 reply

    STeaAnswer
    ST Employee
    December 11, 2024

    Hello @FPasq.1 ,

    If I get you correctly you managed to solve the issue by enabling the DSP extension. if it is the case or you have more details, we can close the thread by marking a reply as solution for better visibility to other uses.
    Regards