STM32H533RE — ThreadX + USBX causes threads to stop cycling
Hello ST Community,
I’m working with the NUCLEO-H533RE. The MCU is feature-rich (three PLLs, robust comms, and onboard USB wired to a USB-C connector) and I’m running the system clock at 250 MHz. I’ve migrated the project to ThreadX (since the old USB stack isn’t provided for this part with FreeRTOS), and the USB stack is the USBX integration.
ThreadX alone comes up clean, but as soon as I enable USBX the application stalls—my threads stop cycling and the system appears to hang. I’m likely missing a configuration detail in the USBX/ThreadX bring-up.
If someone with deep experience on STM32H5 + ThreadX/USBX could point me to the typical culprits (initialization order, memory pools/stack sizes, NVIC priorities/interrupt routing, cache/MPU settings, or any H5-specific gotchas), I’d really appreciate it. Happy to share configuration snippets, clock tree, and MX-generated code if that helps.
Thanks in advance,
Val