STM32H563 MQTT establishing a connection to a remote server
Hello!
I am facing a problem when trying to connect to a remote server using NetXDuo and MQTT. We have a cloud service with which we want to establish a connection so we can send some data. I am basing my project on the example from the STMH573 MQTT Client. The exact problem I am facing is that when trying to establish the connection using the username and password, and the certificates an error occurs, when trying to secure connect. I get these two TSL alerts - alert level is 0x2 and alert value 0x28 (secure connection failed to be established). Using TLSv1.2.
What I did:
- Converting CA certificate to the header file format
openssl x509 -in ca.crt -outform DER -out ca.der
# Then convert into the header file format using xxd.exe
xxd.exe -i ca.der > ca.cert.h- Converting client certificate to the header file format
openssl x509 -in client.crt -outform DER -out client.der
# Then converting it into the header file format
xxd.exe -i client.der > client.cert.h- Converting client key to the header file format
openssl rsa -outform der -in client.key -traditional -out client.key.der
# Then converting it into the header file format
xxd.exe -i client.key.der > client.key.h- Added username and password (those are correct, checked). After the secure connection, error is returned - 0x10005 (NXD_MQTT_CONNECT_FAILURE).
/* Before connecting, send the username and password to log in */
ret = nxd_mqtt_client_login_set(&MqttClient, MQTT_USERNAME, MQTT_USERNAME_LEN, MQTT_PASSWORD, MQTT_PASSWORD_LEN);
if (ret != NX_SUCCESS)
{
Error_Handler();
}
/* Start a secure connection to the server. */
ret = nxd_mqtt_client_secure_connect(&MqttClient, &mqtt_server_ip, MQTT_PORT, tls_setup_callback,
MQTT_KEEP_ALIVE_TIMER, CLEAN_SESSION, NX_WAIT_FOREVER);- From the client example project we have the nx_secure_x509_certificate_initialize function that I used to initialize the CA certificate
ret = nx_secure_x509_certificate_initialize(trusted_certificate_ptr,
(UCHAR*)ca_der, // Pointer to CLIENT CERTIFICATE data
ca_der_len, // Length of the CLIENT CERTIFICATE data
NX_NULL,
0,
NULL, // Pointer to CLIENT PRIVATE KEY data
0, // Length of CLIENT PRIVATE KEY data
NX_SECURE_X509_KEY_TYPE_NONE); // Type of private key
ret = nx_secure_tls_trusted_certificate_add(TLS_session_ptr, trusted_certificate_ptr);
if (ret != TX_SUCCESS)
{
Error_Handler();
}- Then I added another nx_secure_x509_certificate_initialize function to initialize the client certificate and the client key
ret = nx_secure_x509_certificate_initialize(&local_client_certificate,
(UCHAR*)client_der, // Pointer to CLIENT CERTIFICATE data
client_der_len, // Length of the CLIENT CERTIFICATE data
NX_NULL, 0,
(UCHAR*)client_key_der, // Pointer to CLIENT PRIVATE KEY data
client_key_der_len, // Length of CLIENT PRIVATE KEY data
NX_SECURE_X509_KEY_TYPE_RSA_PKCS1_DER); // Type of private key
ret = nx_secure_tls_trusted_certificate_add(TLS_session_ptr, &local_client_certificate);
if (ret != TX_SUCCESS)
{
Error_Handler();
}- Also, enabled the NX_SECURE_ENABLE_ECC_CIPHERSUITE, NX_SECURE_TLS_TLS_1_2_ENABLED, NX_SECURE_TLS_USE_SCSV_CIPHPERSUITE (enabled for testing purposes, did not see anything different) and NX_SECURE_ENABLE_AEAD_CIPHER flags from CubeMX.
- Checked with OpenSSL what kind of cipher is needed - TLSv1.2, Cipher is ECDHE-RSA-AES256-GCM-SHA384.
- Still getting the same alert. Then, if I understood correctly, I need to initialize also the ciphers and the curves
extern const USHORT nx_crypto_ecc_supported_groups[];
extern const UINT nx_crypto_ecc_supported_groups_size;
extern const NX_CRYPTO_METHOD *nx_crypto_ecc_curves[];
ret = nx_secure_tls_ecc_initialize(TLS_session_ptr,
nx_crypto_ecc_supported_groups,
nx_crypto_ecc_supported_groups_size,
nx_crypto_ecc_curves);After all that I am still facing the same problem - unable to establish a connection. What else have I done:
- Checked DNS - working.
- Checked SNTP - working/correct.
- Checked DHCP - working/correct.
- Using openssl to try to establish a connection to the remote server using TSLv1.2 - connection was correctly established, which means that the CA and client certificate, and the client key are correct.
- Using PAHO (Python) to establish the connection with the same credentials - working.
- Converting the credentials to PEM format and then into the header file format - did not work.
- Tried enabling and using TLSv1.3 - same problems/alerts.
Where the program fails is here -
if (client_ptr -> nxd_mqtt_client_use_tls)
{
status = nx_secure_tls_session_start(&(client_ptr -> nxd_mqtt_tls_session), &(client_ptr -> nxd_mqtt_client_socket), wait_option);
if (status != NX_SUCCESS)
{
/* Revert thread priority. */
tx_thread_priority_change(tx_thread_identify(), old_priority, &old_priority);
/* End connection. */
_nxd_mqtt_client_connection_end(client_ptr, NX_NO_WAIT);
return(NXD_MQTT_CONNECT_FAILURE);
}
}returning error code 0x114 (NX_SECURE_TLS_ALERT_RECEIVED) - The remote host sent an alert, indicating an error and closing the connection. This from the nxd_mqtt_client.c file.
I am not sure what else to do and to test. Any help or guidance is appreciated!