STM32H563 TrustZone - USART3 Interrupts Not Working when Non-Secure
Hi,
I'm currently working on a project that uses TrustZone with non-secure peripherals, but I'm having problems with non-secure interrupts.
When I configure USART3 as a secure peripheral in my project, USART3_IRQHandler and GPDMA1_Channel0_IRQHandler interrupts are working fine (in Secure/stm32h5xx_it.c). However, when I configure USART3 as non-secure, these same interrupts don't fire now (now in NonSecure/stm32h5xx_it.c). I verified that the interrupts and DMA are enabled, and that they are included in the NVIC_NS. The USART3 seems to be initialized the right way because using HAL_UART_Transmit works in secure and non-secure modes. However HAL_UART_Transmit_IT and HAL_UART_Transmit_DMA work with USART3 as secure, but not as non-secure.
To deepen my investigation, I wanted to see if the problem was with ALL non-secure interrupts. In a different project, I configured ThreadX as non-secure (using TIM1 as SYS) with the same USART3. The TIM1_IRQHandler is firing, but I get the same problems that the USART3_IRQHandler and GPDMA1_Channel0_IRQHandler interrupts are not firing.
I tried configuring the SAU and GTZC, but I'm new to TrustZone and maybe I'm missing something... I've made sure that the interrupts are marked as non-secure in the partition file:
// <o.29> GPDMA1_Channel0_IRQn <1=> Non-Secure state
// <o.31> USART3_IRQn <1=> Non-Secure state
Can someone help me with this problem or give me some paths towards a solution? I added screenshots of CubeMX configs and the partition file.
Thanks in advance,