STM32H563ZI + APS6404L QSPI Memory Mapped Reads Failing
Hello,
I am using a STM32H563ZI with an external PSRAM QSPI device, the APS6404L. I am using Quad-SPI through the OCTOSPI interface and have been successfully able to get into memory mapped mode. However, every time I go to read, I read out only 0 data. Has anyone ran into this same issue? I have pasted my code for transitioning the device to memory mapped mode and a subsequent test write/read. Thanks!
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_ICACHE_Init();
MX_OCTOSPI1_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_Delay(100);
uint8_t reset_enable[1] = {0x66};
uint8_t rst[1] = {};
uint8_t buff[3];
uint8_t buffer[128], dato;
APS6404_RESET_ENABLE(&hospi1);
PSRAM_ReadID(&hospi1);
APS6404_ENTER_QUAD_MODE(&hospi1);
uint8_t myData[] = {0xD, 0xE, 0xA, 0xD};
APS6404L_QuadWrite(&hospi1, OCTOSPI1_BASE, myData, sizeof(myData));
uint8_t rxData[32];
APS6404L_QuadRead(&hospi1, OCTOSPI1_BASE, rxData, sizeof(rxData));
/* MEM MAPPED MODE */
XSPI_RegularCmdTypeDef sCommand;
XSPI_MemoryMappedTypeDef sMemMappedCfg;
sCommand.OperationType = HAL_XSPI_OPTYPE_WRITE_CFG;
sCommand.Instruction = 0x38;
sCommand.InstructionMode = HAL_XSPI_INSTRUCTION_4_LINES;
sCommand.InstructionWidth = HAL_XSPI_INSTRUCTION_8_BITS;
sCommand.InstructionDTRMode = HAL_XSPI_INSTRUCTION_DTR_DISABLE;
sCommand.Address = 0x00000000;
sCommand.AddressMode = HAL_XSPI_ADDRESS_4_LINES;
sCommand.AddressWidth = HAL_XSPI_ADDRESS_24_BITS;
sCommand.AddressDTRMode = HAL_XSPI_ADDRESS_DTR_DISABLE;
sCommand.AlternateBytesMode = HAL_XSPI_ALT_BYTES_NONE;
sCommand.DataMode = HAL_XSPI_DATA_4_LINES;
sCommand.DataDTRMode = HAL_XSPI_DATA_DTR_DISABLE;
sCommand.DummyCycles = 0; // for reads only
sCommand.DQSMode = HAL_XSPI_DQS_ENABLE;
sCommand.SIOOMode = HAL_XSPI_SIOO_INST_EVERY_CMD;
sCommand.OperationType = HAL_XSPI_OPTYPE_WRITE_CFG;
sCommand.Instruction = 0x38;
sCommand.DummyCycles = 6;
if (HAL_XSPI_Command(&hospi1, &sCommand, HAL_XSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
sCommand.OperationType = HAL_XSPI_OPTYPE_READ_CFG;
sCommand.Instruction = 0xEB;
sCommand.DummyCycles = 0;
sCommand.DQSMode = HAL_XSPI_DQS_DISABLE;
if (HAL_XSPI_Command(&hospi1, &sCommand, HAL_XSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
/* Enable Memory Mapped Mode */
sMemMappedCfg.TimeOutActivation = HAL_XSPI_TIMEOUT_COUNTER_DISABLE;
//sMemMappedCfg.TimeoutPeriodClock = 0x34;
if (HAL_XSPI_MemoryMapped(&hospi1, &sMemMappedCfg))
{
Error_Handler();
}
/* Insert delay 100 ms */
HAL_Delay(100);
volatile __IO uint8_t *mem_addr_byte;
// Writing Sequence (8-bit, unaligned pattern)
mem_addr_byte = (uint8_t *)(OCTOSPI1_BASE);
mem_addr_byte[0] = 0xDE;
if (mem_addr_byte[0] != 0xDE)
{
Error_Handler();
}