STM32H7 Ethernet and LwIP: No data seen when running iperf 2.0.8
Hello,
Question related to post "How to create a project for STM32H7 with Ethernet and LwIP stack working":
I downloaded, build and load the STM32H723_Nucleo_ETH to my Nucleo after I changed the board IP to 192.168.0.160 to fit my network and I run an iperf 2.0.8 (I was not able to find 2.0.6 as mention in the code) on my windows PC with IP 192.168.0.32.
But, I don't see any data on the PC running iperf in server mode on port 5001.
I check with Wireshark also and I don't see data other then a single line:
1225 27.865374 192.168.0.160 192.168.0.34 TCP 60 52432 → 5001 [SYN] Seq=0 Win=5840 Len=0 MSS=1460
Ping from 192.168.0.32 to 192.168.0.160 works fine.
Any help will be appreciate.
Thanks
Eyal