Skip to main content
Visitor II
July 2, 2025
Question

stm32h7 ethernet configration

  • July 2, 2025
  • 6 replies
  • 1246 views

how i am config ethernet in the stm32h753xi6 board ?

    This topic has been closed for replies.

    6 replies

    Super User
    July 2, 2025

    @rockey1 wrote:

     the stm32h753xi6 board ?


    Which stm32h753xi6 board ?

    stm32h753xi6 is just a chip part number - it doesn't identify a board.

     

    Have you searched the Knowledge Base ?

    rockey1Author
    Visitor II
    July 2, 2025

    sorry my mistake i am talking about on stm32h753 chip 

     

    Technical Moderator
    July 2, 2025

    That answer doesn't help much ..

    @rockey1 wrote:

    sorry my mistake i am talking about on stm32h753 chip 


    Ethernet is not UART or SPI, it's a set of complex hardware and software staff.

    So what hardware are you using? and what Ethernet stack you will be using?

    Did you check my previous comment?


    Technical Moderator
    July 2, 2025

    Hello @rockey1 and welcome to the ST community,

    As said by @Andrew Neil stm32h753xi6 is a chip not a board!

    Are you talking about STM32H753_EVAL that contains a STM32H753XIHx? or it's a custom board?

    For the Eval board you can inspire from the examples which are provided in the Cube package using LWIP: https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/STM32H743I-EVAL/Applications/LwIP

    or by referring to this article: How to create a project for STM32H7 with Ethernet and LwIP stack working

    For custom board you need to have the PHY driver.

    Hope that helps.

    Technical Moderator
    July 3, 2025

    @rockey1 

    Could you please provide your STM32CubeMX configuration file (.ioc) so I can verify your setup? Additionally, if possible, please share your schematics and project files. This will help me pinpoint the root cause of the issue and guide you toward a solution.

    rockey1Author
    Visitor II
    July 3, 2025

    Screenshot 2025-07-03 161748.pngScreenshot 2025-07-03 161829.pngScreenshot 2025-07-03 161920.pngScreenshot 2025-07-03 162000.pngScreenshot 2025-07-03 162027.pngScreenshot 2025-07-03 162125.pngScreenshot 2025-07-03 162241.pngScreenshot 2025-07-03 162305.pngScreenshot 2025-07-03 162330.pngScreenshot 2025-07-03 162422.png

    rockey1Author
    Visitor II
    July 3, 2025

    this config and code i am using to run eternet in my stm32h753xi6 chip i am getting this output when i am ping ipScreenshot 2025-07-03 163025.png

    rockey1Author
    Visitor II
    July 3, 2025

    i need a conection between my pc or stm32h753xi6 chip or ping that stm 32 ip and response that is ping that i want only.

    Technical Moderator
    July 3, 2025

    @rockey1 

    Attached below is a working Ethernet project using LwIP and FreeRTOS v1 on the STM32H753ZITx. You can use the Compare Projects tool in STM32CubeMX to compare this working project with your configuration, identify differences, and update your settings accordingly. Similarly, you can compare the rest of the project files to spot any discrepancies.

    Although this example is a UDP echo server, you can certainly modify it to fit your specific needs. For a detailed walkthrough of the steps, please refer to the article linked below.

    Technical Moderator
    July 7, 2025

    Hello @rockey1,

    Do you have any updates regarding your issue? Were you able to resolve it? If so, please remember to mark the response that helped you as a solution by clicking Accept As Solution. This will help other users benefit from the information as well.

    Best regards,